Part Number: CC2591 Other Parts Discussed in Thread: CC2400 , CC2592 Hi! I am using a Ubertooth one, which has a CC2400 and a CC2591 frontend. The question is, how can I get the actual output power of the CC2591? I have checked the CC2591 datasheet but it…
Part Number: CC2400 Hi!
I have a CC2400 chip and I have sucessfully let it run on the analog test mode and the ATEST1/2 seems to output the readings according to the plot in our oscilloscope.
Now I want to collect the I/Q signal wtih a STM32, which has…
Part Number: CC2640R2F Other Parts Discussed in Thread: CC2400 , , CC2500 , CC2640
Hi TI,
We are designing a new product with the CC2640R2F in Proprietary Mode, we need receive the packet from the CC2400. but the CRC seems be different between these two…
Other Parts Discussed in Thread: CC2400 , CC2500 , CC2650 , CC8520 , CC2652R Hi, there,
I seeking a device that provides 1M-2Mbps one way data stream for low latency at 2.4GHz band.
The CC2400 used to fit this purpose, but it is now deprecated. And I've looked…
Part Number: CC2510 Other Parts Discussed in Thread: CC2400 , We are using CC2400 and CC2510 in communication between the vehicle transceiver (tram) and ground (rail switch) transceiver. The vehicle is periodically transmitting radio packets, Ground transceiver…
Hi Tom,
What device (CC2400, CC2500...) are you currently working with?
I think the interface looks strange because of Windows scaling settings, please have a look on the following link: https://superuser.com/questions/1190895/is-it-possible-to-scale…
Part Number: CC2400 Other Parts Discussed in Thread: CC2500 , Hi Champs,
We are using CC2400 base band IC. This chip is NRND. So, According to web page, TI recommend CC2500.
However, this CC2500 pin qty is half of CC2400. Do you have any replacement chip…
Part Number: CC2400 I have a problem with the CC2400 data sheet.
Can you explain how it is possable that the IIP3 is bigger than the 1dB compression point.
According to the data sheet:
Saturation (maximum input level) 3 dBm.
input IIP3 in band -17 dB…
Other Parts Discussed in Thread: CC2400 , CC2650 Hi everyone,
I'm working with my company on the update of an old radio product based on the CC2400 transceiver to a single MCU solution using the CC2650 in proprietary mode. I have been able to write a receive…
Other Parts Discussed in Thread: CC2400 Hello,
Would you please advise the impedance of pins 6,7 and 8 of the CC2400?
Is there any impedance requirements while connecting to those pins?
Please advise.
Thanks.
Jones