Part Number: CC2591
RF: Zigbee
Power: 20dbm
Question: After a month of use, the transmission distance becomes closer, 150 meters => 20 meters
Referring to our test result ,we can confirm that there are some problems with the chip "cc2591" . but…
Part Number: CC2430 Other Parts Discussed in Thread: CC-DEBUGGER Hello,
Regarding to GangPro-CC tool on CC2430F128, my customer is asking a question.
(Question)
They are using GangPro-CC for CC2430 flash writing.
But on only one device, when flash writing…
Part Number: CC2430 Other Parts Discussed in Thread: CC2530 We are trying to use the 2450BM15A0001 balun (from Johanson Technology Inc.) to replace the PCB track balun provided in the TI reference design. The primary reason for this is to reduce size of…
Part Number: CC2430 Other Parts Discussed in Thread: Z-STACK , CC2530 , Tool/software: TI C/C++ Compiler Hi! there. I have a problem with IAR compiler
My hardware choose CC2430-F128 , and I use IAR( 7.6) to compile Z-stack (1.4.2-1.1) 's SampleApp, after…
Other Parts Discussed in Thread: CC2430 with respect to IFA Antenna design. Based on DN007 document, dimension of L1 is 25.58mm, but when we design the Antenna based on dxf document (from CC2430DB), we find the L1 dimension in dxf is 20000+mm, is some…
Part Number: CC2430 SmartRF Studio 7 is not showing "not connected"in the status. Also the menu items are greyed out. I have installed all drivers. There is no Cebal driver showing in Device Manager? I click refresh but nothing show up? I have had the…
Hi Matthew,
Please see CC-ANTENNA-DK-RD Design Files specifically for SWRU120 (this document also includes links to the CC2430 Reference Design files).
Regards, Ryan
CC2430 is obsolete but the OAD process is the same to CC2530. I don’t remember exactly if old Z-Stack provides OAD example for CC2430. If not, you can refer to how CC2530 OAD is done in Z-Stack to implement on CC2430.
Other Parts Discussed in Thread: CC2430 , CC-ANTENNA-DK2 I imported the CC2430 reference design and antenna and using Genesys tool momentum to simulate the input return loss and using the parameter from the PCB, the S11 is looks pretty bad. Hopefully the…