Hi Isaac,
the eZ430-RF2480 is using the obsolete CC2480A1. Depending on your application, you can choose between CC2530 or CC2538 for implementing ZigBee Mesh Network using the Z-Stack.
The SmartRF05EB is like the base board for the CCxxxxEMK daughter…
Shaker:
Is it possible for you start working with CC2530ZNP instead and the new mini kit?
CC2530ZNP Mini Kit http://focus.ti.com/docs/toolsw/folders/print/cc2530zdk-znp-mini.html CC2480: This product is not recommend for new designs http://focus.ti…
Other Parts Discussed in Thread: CC2480A1 , SN75176B Is mounting the XTAL2 (ref.: page 20, http://focus.ti.com/lit/ds/symlink/cc2480a1.pdf) crystal a waste (of money) when operating in UART mode? The processor can not enter low power state when running…
This may warrant a separate thread.
Although dissappointing he MSP430F2274 doesn't meet your application needs, the items I would suggest you review is the following:
CC2480 Data sheet ( http://www.ti.com/lit/gpn/cc2480a1 )
CC2480 Interface Specification…
You can access all of the ZDO functionality "remotely" using MT commands and responses if the ZigBee stack programmed had the correct MT_XYZ flags set when it was built. If you are talking about the CC2480A1 or new ZNP on CC2530, they have it built-in…
Hello Umamahesh,
The best place to start is with the documentation and examples. You can find these if you start using the product pages
http://focus.ti.com/docs/prod/folders/print/cc2480a1.html
http://focus.ti.com/docs/toolsw/folders/print/ez430-rf2480…
Other Parts Discussed in Thread: CC2430 , CC2480A1 I am a little confused by the CTS and RTS pins in the CC2480.
The interface documentation[1] states that:
1) UART Clear to send, CTS (pin 15) is an output.
2) UART Ready to send, RTS (pin 16) is an input…
There is some example software on the eZ430-RF2480 Product folder in the Support Software category.
http://focus.ti.com/docs/toolsw/folders/print/ez430-rf2480.html
In addition, the Z-Accel software product can be found at http://focus.ti.com/docs/prod…
Check the "Reset" example in the CC2480 Sample code examples. Check how the SPI port is initialized and the interface signals configured on startup. http://focus.ti.com/docs/prod/folders/print/cc2480a1.html#toolssoftware CC2480 Software Exam…