Part Number: CC2650 Other Parts Discussed in Thread: CC2500 , CC2510 , CC2652R7 , CC2652RSIP , CC2642R , CC2340R5 , UNIFLASH Tool/software: Hello,
We are in process of shifting from CC2510 to CC2650 considering lower power consumption of the later…
Part Number: CC2500 Our customer GREE is going to send the CC2500 board to detection organization in China. They used seven CC2500 boards to do the micropower wireless test and there is one board whose spurious performance failed the test. The spurious…
Part Number: CC2340R5 Other Parts Discussed in Thread: CC2500 , , CC2510 Hi Champs,
MSK 250kbps: I can select CC2500 COMPATIBLE for whitening.
GFSK 2Mbps: I can only select PN9 for whitening. Does it support CC2500 COMPATIBLE in this PHY configuration…
Part Number: CC2500 I have followed the reference design for the CC2500 balun and pie network to match to a 50 Ohm antenna.
What are the expected losses through these external circuit components ?
After some tuning and improving I see about 11dBm…
Part Number: CC2500 Hi,
We received an inquiry from one of our customers. I can't find an answer from D/S, so please let me know.
1. Regarding sine wave input, it is described as "peak-to-peak amplitude of up to 1V." What is the minimum peak-to-peak…
Part Number: CC2500 Hi Team,
I have a machine here using the CC2500 module that can receive normally at first, but cannot receive after a while.
I switch the mode to transmit, and the module can work normally, but it just cannot receive, and the software…
Part Number: CC2500
Hello everyone. We are using a single CC2500 on a custom board for the transmission and reception of data.
Our intention is to configure the chip with MSK modulation at 2425 MHz. We aim to operate at a 1 kbps data rate with…
Part Number: CC2652P Other Parts Discussed in Thread: CC2500 Hello,
I want to make a wireless connectivity between CC2652 and CC2500. Is it possible? Can someone share the required configurations for both?