Part Number: CC2510 Tool/software: Dear,
I am Giuliano Miccolis, member of the Team Compliance at Vodafone Automotive.
I am contacting you because we need the following MDS:
VODAFONE AUTOMOTIVE p/n: 00IN0021B
TEXAS INSTRUMENTS p/n: CC2510F32RHHR…
Part Number: CC2510 We have planned to use CC2510 device and purchased the device and associated components.
I request two details listed below.
1) There may be change in temperature specification for our system, may be operating temperature
up…
Part Number: CC2510 Other Parts Discussed in Thread: CC2511 , CC2340R5-Q1 , CC2340R5 We need low power SoC wireless transceiver with temperature
range from -55 to +125 deg C,
device like CC2510 is required,
small form factor device is required,…
Part Number: CC2510 1. We are planing a space & power constraint application,
folded dipole cannot be accommodated, whether a chip antenna "2119640001 "
with a miniature balun( may be LDM152G4510EC013) can be used instead of the L & C components …
Part Number: CC2510 Other Parts Discussed in Thread: CC2340R5 , CC2531 , CC2511 , CC2652P , CC2642R Tool/software: Hello,
I need to build a device that will simply communicate over a short distance with another existing device that uses the CC2510.…
Part Number: CC2510 Tool/software: Hey all!
I'm using SmartRF Studio 7 and looking at the registers in the datasheet, becoming familiar with setting them and using them for my cases.
The issue i'm encountering is that 4 of the register sections…
Part Number: CC2510-CC2511DK Other Parts Discussed in Thread: CC2510
Hi Experts,
Good day!
Our customer use a CC2510 component. Now the customer has written a test in order to test the pairing and connectivitie of the component. They use a CC2510…
Part Number: CC2510 I am using IAR Embedded Workbench v8.10.1 and attempting to debug my application on a CC2510F32. I have found that ~20% of the memory addresses in XDATA are read back by the CC DEBUGGER as 0x00; however, I can tell from the execution…
Part Number: CC2510 Hello,
I have made a CC2510 module with Johanson Balun 2450BM15B0003. The two of my modules are able to communicate with each other. At 1 meter, RSSI = -42 dBm (With PIFA Antenna) as per TI design guidelines. But the module is not…