Hi Martin
Please see the CC1110-CC1111DK CC2510-CC2511DK Development Kit User Manual ( http://www.ti.com/lit/swru134 ). Here you will see that the UART_RD is connected to P0_2 and UART_TD is connected to P0_3. From the CC1110 data sheet you will see that…
I would highly recommend that you get one of the kits to have a known good reference system that you can use to test against your own hardware.
The CC2510DK-MINI kit is a nice entry level kit for the CC2510, and it is not very expensive.
You can also…
Hi Igor,
CC2510EM can be used together with SmartRF05EB, meaning that you can plug the EM into the EB and control the radio from SmartRF Studio, program the flash with SmartRF Flash Programmer, use it as a capture device with SmartRF Packet Sniffer or…
Gary,
First of all I agree with what Jim wrote. You can either go for the CC1111EMK solution or the CC1110 Mini DK. The important part that Jim points out is that you will need the CC Debugger to connect SmartRF Studio with both devices. SmartRF Studio…
Martin,
I am working with a CC2510-CC2511DK using the SimpliciTI protocol. In the data sheet for this part, I see mention of a CLKCON register and a OSC field name. In order to set this particular bit in the register the data sheet says CLKCON.OSC=1 or…
Hi,
There are no specific reference designs / applications for ESLs with CC11xx or CC2510. Your questions are mainly oriented towards the system design of the complete ESL and communicating base station. By testing on the development kits then it will…
Other Parts Discussed in Thread: CC2511 , CC2510 , REMOTI , CC2530 , CC2531 , CC2533 , SIMPLICITI Hi To All,
I'm struggling to design a link between my CC2510 and the USB receiver CC2511.
I have the CC2511DK_dungle and one CC2510DK-MINI kit. The example…
Other Parts Discussed in Thread: SIMPLICITI , CC2510 , MSP430F5438A Hi there,
I have just downloaded SimpliciTI v1.2.0 and tried to run the Simple Peer-to-Peer example code on the CC2510 SoC. The compiler that I am using is the IAR EW8051 v8.11. I can run…
What you are looking for sounds a bit like the software example called "rf_modem", as one of the USB examples for pairing (CC2511 USB dongle) + (CC2510EM + SmartRF04EB). You can find it as "CC USB Firmware Library and Examples" on e.g. the …