Other Parts Discussed in Thread: CC2510 , CC2500 Hi,
I'm from University and we have ordered "minimum package to use packet sniffer for cc2510 devices" - we received CC2511DK USB dongle. According to user manual it should be already programmed to be…
Hi,
Where can i get the IAR files for the Rs232 to USB example?
When you download the zip file with the example, currently rev C, from e.g. the CC2510-CC2511DK development kit page:
CC USB Firmware Library and Examples (Rev. C) (zip 1316 KB) 8468 …
Other Parts Discussed in Thread: CC2511 , CC2510 Hi
I just got the CC2511DK few days ago. I plugged the evaluation module into the evaluation board and programmed the chip on the evaluation module with the example PER_TEST provided by TI. It works correctly…
Richard Norris said:
It will be interesting to find out whether we can achieve what we need to with SimpliciTI; if we are able to tweak the code though, that may give us the flexibility we may eventually require. I'm hoping to keep the networking simple…
Other Parts Discussed in Thread: CC2531 , CC2530 , SIMPLICITI , CC2510 , CC2511 Hi All,
IAR Systems recently released Embedded Workbench for 8051 version 7.51A. The product page at http://www.iar.com/ew8051 is now updated with information about new features…
Hi Ajay,
Sustainable data rate is less than 200k bits per second, so video is not going to be plausible.
1. CC2511 and the CC1111 are both Single Chip USB devices.
2. Both the CC2511 and the CC1111 are both available to non-tier 1 suppliers.
3. The range…