Other Parts Discussed in Thread: Z-STACK , CC2530 The current code writes all Zigbee node types in the .cfg file. You can choose the corresponding .cfg file for burning to select the desired type directly. Is there a way to wirelessly control Zigbee end…
Part Number: CC2530 Other Parts Discussed in Thread: CC2591 , , TIMAC , SIMPLICITI , CC1352P , CC2652P
Hi everyone,
I am using CC2530 + CC2591 and BasicRF (from the CC2530 examples) to comunicate 3 devices. The RF setup is simple: broadcast messages…
Part Number: CC2530-CC2592EM-RD Other Parts Discussed in Thread: CC2592 , CC2530 Hello,
I would like to get a design review done for one of my designs based on the CC2530 with the power amplifier CC2592 and a chip antenna from Johansson Technologies…
Part Number: CC2530 We are updating zigbee stacks on a ZNP based coordinartor as a part of a gateqway. In 2.5.3 Stack everyting is waorking fine. Bou in 2.6.x version I noticed tha AF_INCOMING_MSG is received with "extra fileds" after the data field.…
Part Number: CC2530 Other Parts Discussed in Thread: Z-STACK
Hi guys,
I have my ZED based on Z-stack 3.0.2
I have NWK_AUTO_POLL enabled
In init function I call: bdb_StartCommissioning(BDB_COMMISSIONING_REJOIN_EXISTING_NETWORK_ON_STARTUP);
and…
Part Number: CC2530 Other Parts Discussed in Thread: CC2592 , , Z-STACK Hi,
About CC2530+CC2592 Zigbee Solution, it need CE certification compliance.
When Channel TX power = 10dBm, Max PSD will be 9dBm/MHz;
When Channel TX power = 20dBm, Max PSD…
Other Parts Discussed in Thread: CC2530 , Z-STACK , CC2531 HW : CC2530 SW : Z-Stack 3.0.2 Compiler : IAR 10.30 Coordinator : Zigbee2MQTT
THE BASICS : I am working with some CC2530 devices that act as End Devices and connect to a network provided by…
Part Number: CC2530 Other Parts Discussed in Thread: Z-STACK , SIMPLELINK-CC13XX-CC26XX-SDK Hi,
We are running our lighting applications on cc2530 zstack, we use osal timers for lot of our features.
Recently observed that osal_systemClock is getting…
Part Number: CC2530 Other Parts Discussed in Thread: Z-STACK Hi,
We are running our lighting applications on cc2530 zstack.
I wanted to profile memory usage metrics and got good amount of metrics, like this below. I am printing it via UART.
Memory…