Other Parts Discussed in Thread: REMOTI , CC2530 Hi,
I got the remoTI DK last week. I'm trying to figure out if there is a way to interface the remote and CC2530/2531 with a non RF4CE device - specifically a home entertainment device such as a TV, DVD…
The RemoTI RF4CE protocol stack is only built by the IAR compiler, and from their website, it does not look like it runs on a Linux box:
To install and run the IAR Embedded Workbench, you need the following:
If you want to write a sample application…
Other Parts Discussed in Thread: REMOTI Hi,
Does the answer in this thread "CC2530: What is the advantage of using a 32kHz crystal vs. internal RC oscillator?" also apply for the RemoTI RF4CE stack? I.e. is it a requirement to use an external…
Other Parts Discussed in Thread: CC2530 , Z-STACK , CC2430 Hi, everyone
I'm david
I hope your help
CC2530 suppots both the Zigbee pro 2007 and RF4CE stacks
I saw that CC2530 Large Network Demo Zigbee Pro stack (Z-stack 2.2.0) supporting 94 devices using…
Other Parts Discussed in Thread: CC2530 , CC2590 , Z-STACK , CC2591 , CC2592 , CSD Hi Guys,
I´m working to configure Ebyte Module E18-MS1PA2 CC2530 (w/ PA and LNA inside), but I didn´t have success to setting it correctly. According the Ebyte datasheet is necessary…
Part Number: CC2640R2F Other Parts Discussed in Thread: CC2530 , CC2541 , CC2640 We have a new project that requires a BT chip that application firmware coding has direct access to low level radio. The reason of direct low level radio is to guarantee the…
Dear Yikai,
I have downloaded the RemoteTI but it does not have IR code in it.
Also I am unable to understand how to use ZigBee RF4CE with CC2530? Are there any specific document to guide me in using ZigBee RF4CE?
Other Parts Discussed in Thread: CC2530 I have one question regarding using WIFI/BT/Zigbee altogether and using CC2530 for ZigBee. In RF4CE protocol, Frequency Agility function is included as mandatory. If CC2530 RF4CE is used, I’m wondering if channel…
Part Number: CC2531 Other Parts Discussed in Thread: CC2530
I am attempting to run some simple code on the CC2531 to prove that I can control some basic things from the chip before trying to run the same code on a CC2530 on our custom board.
I started…