Part Number: CC2530-SE2431L Other Parts Discussed in Thread: CC2530 , Z-STACK Tool/software: TI C/C++ Compiler I can't understand this error (........hex used for multiple files) and how to solve it.
what these warning mean??
//////////////////////…
Part Number: CC2530-SE2431L Other Parts Discussed in Thread: CC2530 , , Z-STACK Hello, I bought a radio transmitter for RC hobby. It's FrSky's Taranis Q x7.
The problem I'm facing is I would like to change it's transmission power. From what I've…
Hello,
Do you know if P1_0 is redefined anywhere in the code and set to tristate? Currently my customer has P1_0 set as the output and pulled low which it is supposed to be. But he has his ANT_SEL working incorrectly and selecting Antenna 2 instead of Antenna…
Part Number: CC2530 Dear Team
Good day!
Our customer want to confirm that, if CC2530 can support external PA to enhance transmission distance .
if so, what’s the suggestion PA spec or part number? Any user guide?
And I find a reference design which…
Other Parts Discussed in Thread: CC2530 , CC2590 , Z-STACK , CC2591 , CC2592 , CSD Hi Guys,
I´m working to configure Ebyte Module E18-MS1PA2 CC2530 (w/ PA and LNA inside), but I didn´t have success to setting it correctly. According the Ebyte datasheet is necessary…
I was referencing this design: www.ti.com/.../CC2530-SE2431L
I know its not sub 1g. I was hoping for an FEM with a built in duplexor, but I think usually there is a switch on for RX and TX not a duplexor. Just wondering if you had anythoughts?
The…
processors.wiki.ti.com/.../LNA_with_Z-Stack-Home-Automation-1.2.1 There in the link I see Z-Stack-Home-Automation-1.2.x supports the Skyworks SE2431L PA/LNA with CC2530/1/3 and SE2431L is currently not supported with the CC2538 RF-SoC
Regarding CC2530-CC2592EM vs CC2530-Skywork-SE2431L: It depends on your requirements.
Performance (sensitivity/ output power) is one spec point but also price (CC2592 vs SE2431L) and PCB area etc.
The two designs are not the same, you have to compare…