Part Number: CC2531EMK Hi,
I have a dongle USB that works as a coordinator and has two end-devices connected to it.
Is there any way to get the list of IEEE Addresses of the devices connected to the network, instead of the Network Address?
Part Number: CC2531EMK Hi,
I've realized that after sending multiple commands at once, the AF_DATA_REQUEST_SRSP responds with a 0x11 status; that looking at the zstack.h file it means that the buffer is full.
In my source code (below the code snippet…
Part Number: CC2531EMK Hi,
I have a Danfoss Thermostat connected to my coordinator.
I also have the ZigBee Cluster Specification of the thermostat. ( Link )
I've tried to use AF_DATA_REQUEST
<TX>12:37:03.48 COM4 AF_DATA_REQUEST (0x2401)
…
Part Number: CC2531EMK Hi,
I saw, via ZTool, that BDB_START_COMMISSIONING in Network Steering runs a permit join.
But I would like to know for how many seconds does it open the network.
Thanks in Advance.
Part Number: CC2531EMK Other Parts Discussed in Thread: CC2531 Hi,
Part number which is mentioned in BOM list of CC2531 is not found on webiste.
Even alternate part number is wrong and that is given for Type B while on dongle it is USB Type A. …
Part Number: CC2531EMK Hi,
I managed to connect my danfoss thermostat to my CC2531EMK ( I follow this blog's post: Sun May Sky: Use ZTool + Z-Stack 3.0 ZNP to set up a basic Zigbee 3.0 network )
I sniffed the serial port, which is connected to my…
Other Parts Discussed in Thread: CC2531EMK Hi We are planning to use CC2531EMK and CC1111EMK for sniffing 2.4Ghz and 868Mhz for mass deployment(approx 180quantiy). Requirement : can we create multiple threads; to access multiple sniffing dongles at the…
Part Number: CC2531EMK Other Parts Discussed in Thread: FLASH-PROGRAMMER , CC2531 , , PACKET-SNIFFER , CC-DEBUGGER When starting SmartRF Packet sniffer software I get a SnifferAgent error: Autostart Warning "No devices are running as expected. Please…
Part Number: CC2531EMK Hi,
I've bought an used IKEA Tradfri Repeater and after I reset it, by following the Manual I paired it to my coordinator, a CC2531EMK with ZStack 3.0 flashed on it.
Looking via ZTool I can see a ANNCE_IND with the network address…