Other Parts Discussed in Thread: CC2533 We made a RF4CE 2.0 RC base on CC2533F96 chip solution , throught the data sheet we see the chip work votage rang from 2.0V~3.9V.
But we find that the CC2533 RC can not work under 2.3V voltage. This is SW issue or…
Part Number: CC2533 Other Parts Discussed in Thread: CC2541 , , CC2543 Hi guys,
I'm using a CC2533F96 to communicate (SPI master) with an external flash (SPI slave). When I use USART1 Alt. 2 (MISO P1.7 MOSI P1.6 SCLK P1.5), I'm able to get the manufacturer…
Part Number: CC2533 Is it possible to use the same USART (0 or 1) with UART and SPI settings at the same time?
For example:
USART0 UART Alt. 1
RX P0.2
TX P0.3
and
USART0 SPI Alt. 2
MOSI P1.5
MISO P1.4
SCLK P1.3
SS P1.2
??
Part Number: CC2533 Hi,
Is it OK to use the external 32 MHz oscillator instead of the 32 MHz crystal?
If yes, could you, please, give some recommendation (signal level, etc).
Part Number: CC2533 Other Parts Discussed in Thread: CC2620 Hi,
I need to revisit the issue I had in this thread: e2e.ti.com/.../508596
We need to be able to discovery more than 10 devices.
Is there anyway to recompile or hack the library to allow more…
Other Parts Discussed in Thread: CC2531 , CC2533 We make the RF4CE RC by CC2533 chip base on RemoTI-CC253xDK-1.4.0 SDK, we do continuous paring test(ZRC2.0, key validation mode ) with CC2531 dongle on PC , the fail rate among 5%~10%.
There are 2 types error…
Part Number: CC2533 Hello Champs,
One question popped up from customer side, regarding CC2533 Interrupt edge detection voltage level..
Customer application have tilt sensor(analog level) and it is connected to I/O port interrupt in CC2533 and detect falling…
Other Parts Discussed in Thread: CC2533 Dear Champs,
Do we have the PCB Layout File for CC2533 Evaluation Module?
It's better in Altinum Design format.
I looked at the webpage below, but it seems there is not such file....
http://www.ti.com/tool/cc…
Hello Bun,
As suggested, PFA the review request form filled to proceed with the review.
Please help on priority.
Copy of SimpleLink_24GHz_Design_Review_Request_Form.xlsx 7723.schematic_for_review_ti_CC8530.pdf