Part Number: CC2538-CC2592EM-RD Other Parts Discussed in Thread: CC2538 Hi,
We have a board that copies the reference design as closely as possible with the exception that the SMA SMT connector was changed to a through-hole mount to reduce breakage…
Part Number: CC2538-CC2592EM-RD Other Parts Discussed in Thread: CC2592 The two traces on the output side of the CC2592 are different widths and have different characteristic impedances.
Both the SMA-connected device and the IFA are 50Ω loads.
1.…
Part Number: CC2530-CC2592EM-RD Other Parts Discussed in Thread: CC2592 , CC2530 Hello,
I would like to get a design review done for one of my designs based on the CC2530 with the power amplifier CC2592 and a chip antenna from Johansson Technologies…
Part Number: CC2538-CC2592EM-RD Other Parts Discussed in Thread: CC2538 , CC2592
Can I use cc2592 for both TX and RX communication in the same device. We designed 2 devices one (Device A) is based on cc2538 EM and the other one based on cc2538-cc2592…
Part Number: CC2538-CC2592EM-RD Other Parts Discussed in Thread: CC2538 , CC2592 , Z-STACK , CC2531 , CC2530 , CC2530EM I am using cc2538 and cc2592 on a custom designed board to transmit data to a zigbee node (whose mac address is hardcoded in the application…
Part Number: CC2538-CC2592EM-RD Other Parts Discussed in Thread: CC2592 , Z-STACK , CC2538 , CC2530
I am using a CC2538+CC2592 based custom board running a modified SampleSwitch application (Z-Stack Home 1.2.2a.44539), Coordinator configuration.
End…
Part Number: CC2530-CC2592EM-RD Other Parts Discussed in Thread: CC2592 , CC2530 I want to test the S11 of CC2530+CC2592 RF TX and RX chain.
Use SmartRF Studio 7 to set TX or RX mode for CC2530+CC2592, how to confirm if CC2592 is working at a right…
Part Number: CC2538-CC2592EM-RD Other Parts Discussed in Thread: CC2538 , CC2592 My application code is to be run on a custom design based on cc2538 and cc2592. The application code executes just fine and i can step into the code at any point.
Because…
Part Number: CC2538-CC2592EM-RD Other Parts Discussed in Thread: CC2538 This might not be the right forum/heading for this question. Admin/Moderators please move the thread to relevant section if needed.
Well we are on the verge of completion of functionality…
Part Number: CC2530-CC2592EM-RD Other Parts Discussed in Thread: CC2530 Hello, I am currently using CC2530 ZNP (3.0.2), because there are some issues, so I want to turn off the zigbee CSMA/CA mechanism, but I don’t know how to turn it off or how to modify…