Part Number: CC2538-CC2592EMK Other Parts Discussed in Thread: CC2340R5 Hi TI Team,
I am reaching out on behalf of our engineering team as we are currently in the process of integrating a Zigbee antenna/module into our access control door lock system…
Part Number: CC2538-CC2592EMK Other Parts Discussed in Thread: CC2538EMK , CC2538 Tool/software: hello Team,
1] i am working on CC2538EMK . there is on chip ADC but when i was given analog input to ADC it will give offset in data sheet there is offset…
Part Number: CC2538-CC2592EMK Other Parts Discussed in Thread: CC2538 , MAX3223 Tool/software: hi team ,
am designing a custom board based on the CC2538 microcontroller, and I would like to share the UART communication configuration . The setup involves…
Part Number: CC2538-CC2592EMK Other Parts Discussed in Thread: CC2538 Tool/software: hi team,
i am working with cc2538 am using external SPI flash IS25LP128 so how can i congifure for read and write operation and also suggest refrance code for that
Part Number: CC2538-CC2592EMK Other Parts Discussed in Thread: CC2538 Tool/software: hi team , i am working with CC2538 , i am tring to implement CTS RTS logic the logic of CTS RTS is when transmitter send RTS low then at reciver side on cts pin it recive…
Part Number: CC2538-CC2592EMK Other Parts Discussed in Thread: CC2538EMK Tool/software: hi TI , i want to use SPI NOR flash in cc2538EMK so how can i use . and also explain what is SPI NOR flash
Part Number: CC2538-CC2592EMK Other Parts Discussed in Thread: Z-STACK , CC2538 Hi, Greeting of the day!!.
What I want to do, I have two kit's of CC2538-CC2592EMK and want to communicate between them via host micro-controller over UART and some type…
Part Number: CC2538-CC2592EMK Other Parts Discussed in Thread: CC2538 , Z-STACK , CC2592 , CC2590 I want to amplify the original CC2538 output power, so I bought CC2538-CC2592.
I download my original code, and test the output power, it is only -94…
Part Number: CC2538-CC2592EMK
SmartRF Studio, the device control panel can not open.
cc2538-cc2592 Evaluation Module Kit mounted to SmartRF06EB, which is connected to windows PC (SmartRF 7 2.28.0 version).
The board can be detected, but can not…