Part Number: CC2545 HI,
i connected cc2545 to cc debugger it is showing the green color LED but in IAR target selection window is appeared. and in device manager
but same debugger and same version IAR are working fine for another PCB both have same…
Manikanta,
Yes, the CC2545 can operate fine outdoors, no issues.
1) Board X, you need to verify the center frequency and the output power of the custom design in conducted mode (using coaxial wire to test equipment). I also recommend confirming…
Part Number: CC2545 dear all:
My project is in use CC2545,The length of data per packet is greater than 128 bytes,How to do it correctly to send and receive data correctly
thanks!
Part Number: CC2545 Hello,
according to TI routine, there are problems in simulation debugging. How to set it? When debugging step by step, it suddenly can't stop. the issue as below:
thanks.
Part Number: CC2545 Other Parts Discussed in Thread: CC2530 , CC2592 , CC2541 , CC2590 , CC2538 Hi,
I am planning on using C2545 in one of my projects. Please share any info on the range extender reference design that can be used for CC2545 chip.
…
Part Number: CC2650 Other Parts Discussed in Thread: CC2545 , , CC2640R2F Hi,
Developing with the CC2545 today we may want to move to the CC2650/CC2652 in future products. Just want to double check that the device RF portions should be interoperable…
Other Parts Discussed in Thread: CC2545 help please
i use CC2545 in a remote board
we need pass through SRRC,
in the following three band,we fail
our crystal is 32M
how to debug this question?
Hi Hassan,
The frequency step size is 1 MHz, as described in the text you copied from the User Guide. This is independent of data rate.
Cheers,
Fredrik
Other Parts Discussed in Thread: CC2545 Hi sir,
Using Auto mode in CC2545 the packet structure as follows:
Statement: The communication will achieved between Transmitter and Receiver when the Address entry and address field is matched.
Is the…