Part Number: CC2545 Hello~
I use CC2545 basic mode to design my application.
I find a problem and I cannot resolved it over 3 weeks.
The situration as below
1packet is 128byte. TX first byte is 0x7F
RF datarate is 2M, 500K deviation.
In 5ms TX transmit…
Part Number: CC2545 Hello,
according to TI routine, there are problems in simulation debugging. How to set it? When debugging step by step, it suddenly can't stop. the issue as below:
thanks.
Part Number: CC2545 HI,
i connected cc2545 to cc debugger it is showing the green color LED but in IAR target selection window is appeared. and in device manager
but same debugger and same version IAR are working fine for another PCB both have same circuit…
Part Number: CC2545 dear all:
My project is in use CC2545,The length of data per packet is greater than 128 bytes,How to do it correctly to send and receive data correctly
thanks!
Part Number: CC2545 Other Parts Discussed in Thread: CC2592 Hi all,
I was designed 2 different boards with cc2545 chips.
In one board(Board X) I used CC2545 chip and cc2592 PA.
In another board(Board Y) I used CC2545 Chip and Balun IC and chip antenna…
Part Number: CC2545 Other Parts Discussed in Thread: CC2530 , CC2592 , CC2541 , CC2590 , CC2538 Hi,
I am planning on using C2545 in one of my projects. Please share any info on the range extender reference design that can be used for CC2545 chip.
Any help…
Part Number: CC2650 Other Parts Discussed in Thread: CC2545 , , CC2640R2F Hi,
Developing with the CC2545 today we may want to move to the CC2650/CC2652 in future products. Just want to double check that the device RF portions should be interoperable with…
Part Number: CC2545 Dear All,
According to TI CC2545 User Guide Page 236, Section : 23.5 Frequency and Channel Programming:
"
For normal transmit and receive tasks, the carrier frequency is set by using the register PRF_CHAN.FREQ. The carrier frequency…
Part Number: CC2545 Hello,
We are manufacturing in volume a system that consists of a base station and a remote node, both of which use the CC2545 for point to point communications. On most of our systems we see good performance. However, on a small number…
Other Parts Discussed in Thread: CC2545 Hi all,
Can any one provide the solution for the following question:
1)what is the SNR or noise margin of the CC2545 radio?