Other Parts Discussed in Thread: CC2592 , CC2545 Hi all,
I Interfaced the CC2592 to CC2545 as follows:
PA_EN pin to P1.0 in CC2545
LNA_EN Pin to P1.1 in CC2545
HGM Pin to P2.0 In CC2545
I established a communication between two CC2545 Chips both as transceivers…
Other Parts Discussed in Thread: CC2545 help please
i use CC2545 in a remote board
we need pass through SRRC,
in the following three band,we fail
our crystal is 32M
how to debug this question?
Other Parts Discussed in Thread: CC2545 Hi sir,
Using Auto mode in CC2545 the packet structure as follows:
Statement: The communication will achieved between Transmitter and Receiver when the Address entry and address field is matched.
Is the above statement…
Other Parts Discussed in Thread: CC2545 , CC2592 Hi all,
I am trying to read the RSSI register value in cc2545 and i am getting a value of 0x09. I can see that that i am always getting the same value either with or without antenna.what does it indicate…
Remainder:
In reply to TA12012 :
Hi TA12012,
I am using the IAR embedded work bench IDE.
I was configured all the devices in auto mode. I think there was no option for using of Streaming protocols. I observed the following protocols in user manual:
In…
Hello Bun,
As suggested, PFA the review request form filled to proceed with the review.
Please help on priority.
Copy of SimpleLink_24GHz_Design_Review_Request_Form.xlsx 7723.schematic_for_review_ti_CC8530.pdf
Other Parts Discussed in Thread: CC2545 Hi all,
Please verify the attached pic.
can I replace the balun IC (LFB182G45BG2D280) or not which is manufactured by Murata Electronics.
Other Parts Discussed in Thread: CC2530 , CC2545 , CC2538 hi sir, 1)when I was connecting the cc debugger to cc2530 module ,the led in cc debugger glows in green color and it was connected. when it will connected to cc2545 module ,the led glows in red color…
Other Parts Discussed in Thread: CC2650 , CC2540 , CC2545 Hi,
I want to read the value of the RSSI register 0x618E in CC2545. This register is within the RF core. So I am wondering is it possible to read it or not. When I use CC2540/CC2650, the registers…
Part Number: CC-DEBUGGER Other Parts Discussed in Thread: CC2541 , CC2540 , CC2543 , CC2545 , CC2544 , CC2533 , CC2530 , CC2531 , CC2511 , CC2510 , CC2431 , CC2430 Hello Team,
Is there a is way to use a 10-pin CC debugger on a 14-pin JTAG?
Regards,
Renan