Other Parts Discussed in Thread: CC2545 , CC2530 , CC2541 , CC2543 , CC2544 we were been facing problems in throughput of CC2530 as it is TI MAC and Zigbee stack ,typically the data rate is maximum 250Kbps and hardly we are getting a throughput of only 50Kbps…
Other Parts Discussed in Thread: CC2545 Hello,
I am using a pair of CC2545's in Basic mode with 255 Byte packets, 2Mbs, 13 Byte Preamble, AGC on, 32 Byte Sync word. I have a tight loop that transmits a request for 'next data' and then receives a 255…
Other Parts Discussed in Thread: CC2545 Greetings.
I have been having trouble with off-SOC communication with the CC2545. I am using the CC2545EM evaluation module and programming with the CC debugger.
I have tried SPI/I2C/UART and all three are having…
Hello Mike,
Sorry for the late response.
For switching on the same channel (with or without different IF frequency on TX/RX):
The start-up time is constant with a very small deviation. The 130 us is a value set which is used in auto-mode (radio switch automatically…
Other Parts Discussed in Thread: CC2545 , SIMPLICITI , CC2543 , CC2540 , CC2541 , CC2533 I ordered two CC2545EM modules and I am trying to install them on SMARTRF05 board. I am trying the setup for peer-to-peer application.
Followed :
http://e2e.ti.com/ sup…
Part Number: CC2543 Other Parts Discussed in Thread: CC2545 team,
My customer plan to use CC2543 to design a 2.4GHz 'flip pen' to control PPT in presentation.
Is it a good device to choose here?
And also I see that the CC2545 EVM link in ti.com…
Part Number: CC2543 Other Parts Discussed in Thread: CC2544 , CC2545 Hi,
I'm testing power consumption of CC2543 in power mode PM2 with sample code from TI , i found that:
- As data sheet say that about CC2543, Power mode 2 (sleep timer on): curren…
Hi Peter,
No, there are no similar components without the radio. If the application size is small when the BLE Stack is removed, you can consider the CC2543 or CC2545 instead.
Regards,
Fredrik