Part Number: CC2564C Hi TI,
Is there any way we can control the timing parameters of SCO/ eSCO connections, eg D-parameter , T-parameter etc.
Thanks!
Vishnuprasad
Part Number: CC2564CSTBTBLESW Other Parts Discussed in Thread: CC2564 Tool/software: I'm working on project which using CC2564 + STM32F4 device, I need to adding RF test mode or BLE DTM test mode.
following the CC256x Testing Guide, Service pack must…
Part Number: CC2564C Hi,
We are building a Linux based solution using AM6231 and plan to use BlueZ with CC2564C as BLE controller, is it possible?
Regards,
Yadhu
Part Number: CC2564C Hi TI,
We are working on a Product which use Dual mode feature of CC2564C (BT+BLE).
We like to set up one production line Testing system, So that we can make sure the RF part is working as expected.
From the FCC Testing guides…
Part Number: CC2564C Tool/software: Hi Team,
Connection capabilities of the CC2564C Dual-Mode Bluetooth® Controller when functioning as a slave device(BR/EDR).
1. As a master, I can connect up to 6 active slave devices. 2. However as a slave, it is…
Part Number: CC2564C Hi Team,
We would like to use CC2564C (BLE 5) in our design having STM32H series MCU.
Can we use the same stack as STM32F series - link ?
If not, Can you please suggest an appropriate stack?
T&R,
Akshay
Part Number: CC2564C Other Parts Discussed in Thread: BL6450 Hi,
since last week we have been testing the integration we did with our product (custom board based on Jacinto running Android 8.0) of the CC2564C controller. Although we did the integration…
Part Number: CC2564C Other Parts Discussed in Thread: MSP-EXP430F5529LP Tool/software: HI team
I have a cc2564cQFN-EM and msp-exp430f5529LP board, how to do hardware connections to work with it(flash and connectivity).
please suggest a way for it…
Part Number: CC2564C Other Parts Discussed in Thread: CC2564 Hi team,
Here's a request from customer:
As the title says, does CC2564C support RF frequency calibration?
Can you help for checking this point?
Thanks and Regards,
Nick
Part Number: CC2564CSTBTBLESW Other Parts Discussed in Thread: CC2564C Tool/software: Hello,
In our application we use version 5.1.1.1 of the stack.
We perform the Inquiry from a PC, and expect to find our machine, equipped with the BT module, in…