Part Number: CC2564MODNEM Hello TI Support,
We are intending to use Bluetopia stack with MSP430 and CC2564MODNEM chip. This is a medical device and on our MSP430 chip we are using our own home grown Real Time Operating System /Kernel.
I have gone…
Part Number: CC2564MODNEM Hello,
I have the same Issue as described in the question: http://e2e.ti.com/support/wireless-connectivity/bluetooth/f/538/p/861034/3186729#3186729
The Eval board isn't defect because I can start some commands from the library…
For some reason the default stream mode is sink so the first connected device is the sink and the second is the source.
So now the reapeater works, in the future we may have to change this behaviour but for now it is acceptable.
Thanks a lot,
Jo
Hi Manuska,
I am closing this thread due to inactivity. If you have a new issue please create a new thread. If you have the same issue please respond to my question here.
Jesu
Jo,
Jo Laf said: First question is this only possible ? The following post on this forum make me think it is :
Yes, this is possible when using the unassisted A2DP and a high enough UART baud rate (for example 2 Mbps or higher).
Jo Laf said: Second…
Hi,
For some reason the 0 ohm resistors were wongly placed on the CC256XEM-STADAPT.
I first thought it was ok as the pdf says the EVAL mode is the default configuration.
Thanks a lot,
Jo
Part Number: CC2564MODNEM Other Parts Discussed in Thread: WL18XXCOM82SDMMC I am trying to initialize the evaluation board with the provided service pack (BLE script) with the HCI tester tool, however, the script does not run and there is no "incoming…
Part Number: CC2564MODNEM I use HCITest to initialize the CC2564MODNEM and set BT module in test mode.
(1) 'Send’ HCI commands and only ‘Wait’ the response of ‘0xFF36’ --- the initialization is also completed and function well.
(2) 'Send’ HCI commands…