Hi Kozo,
The CC2564MODA supports WBS and NBS HFP over PCM interface. For implementation, please refer to the HFPDemo_AG and HFPDemo_HF in the CC256XMS432BTBLESW or the CC256XSTBTBLESW.
Also, the hardware setup for the CC256XMS432BTBLESW includes the…
Part Number: CC2564 Other Parts Discussed in Thread: BT-MSPAUDSINK , , CC256XMS432BTBLESW , CC3200AUDBOOST I got a BT-MSPAUDSOURCE EVM , after open box, I follow USER GUIDE and try to demo it. But I have two different BT HEADPHONE, can't find them iby EVM…
Part Number: CC2564MODA Other Parts Discussed in Thread: CC256XMS432BTBLESW Tool/software: Code Composer Studio Hello there,
I recently start using the MSP432P401R LaunchPad with the BOOST-CC2564MODA plug-in module.
I'm testing some of the examples …
Hi Aleksei,
Aleksei Makalov said:
This error stands for BTPS Error Feature Not Available. Regarding this error on e2e.ti.com, developers say that this feature is not supported by Bluetopia SDK libraries for MSP430.
1. Can I implement HFP AG on the CC…
Angelo,
The MSP-EXP430F5529LP + BOOST-CC2564MODA is not a suitable hardware setup for HFPDemo since the MSP430F5529 does not have enough flash to fit the entire demo.
The MSP-EXP432P401R + BOOST-CC2564MODA + CC3200AUDBOOST is the correct hardware setup…
John,
The ti dual mode bluetooth stack in the CC256XMS432BTBLESW SDK is only for non-threaded systems. Thus, there is no example included in the SDK that uses TI-RTOS kernel.
If your application defines and uses a custom GATT based profile, you can take…
Part Number: CC2564 Other Parts Discussed in Thread: TLV320AIC3100 , TLV320AIC3254 , CC256XMS432BTBLESW Hi,
I'm using cc2564B connected in assisted mode to TLV320AIC3100, for HFP profile.
Is mSBC codec supported in this hardware configuration?
Is there…
Part Number: CC2564MODA Tool/software: Code Composer Studio Hi,
I'm currently using the bluetooth stack for the CC2564MODA, available here http://www.ti.com/tool/CC256XMS432BTBLESW, and using with the MSP432P401R Launchpad Dev Kit. I need to use it…
Hi Paolo,
The error -103 above refers to the BTPS_ERROR_FEATURE_NOT_AVAILABLE. Please note that some of the old Bluetopia releases like MSP430 and TIVA do not have HFP Demo in Audio Gateway (AG) role. These SDKs do not support HFP AG role and they only…
Hi,
I think there is a bug in the SPPDemo software for MSP432 ( CC256XMS432BTBLESW ) that doesn't allow the user to configure baudrates greater than 115200. The problem might be in the following line from SPPDemo.c
MaxBaudRate = (DWord_t)(HCI_DriverInformation…