Other Parts Discussed in Thread: CC2571 Just thought I'd toss this one out as well. Anyone with a use case that requires high network flexibility, vast node density, or just ubiquity of ANT+ devices might be interested in this announcement :)
http…
Hi Harrison,
Can you confirm that the CC2571 experimenter board is standard to the other ANT dev kits, and not to the CCxxxx daughter cards that plug into TI's microcontroller eval/dev boards? I'm looking pretty hard at ANT right now, although the…
Other Parts Discussed in Thread: CC2571 , MSP430BT5190 Hi, I would like to develop wireless bridge chip based solution to an ANT device. I need it to be low cost and low power consumption. I want to use TI’s CC430 as the RF module combined with the CC2571…
Hi All
I think I can suggest a very viable solution using the TI CC2571.
This chip is pin compatible with the CC2540 and contains the ANT protocol which supports a very usefule practical mesh environment.
The CC2571 as it sits now, supports multiple…
Other Parts Discussed in Thread: CC2571 , CC2567 , CC2570 I know that TI's CC2571 can handle 8 channels of ANT. How about the CC2567? Is there any way it can be configured possibly using the MSP430 to handle multiple channels?
Hi Mike,
I can only make a few suggestions, the CC2571/CC254x share virtually identical RF front ends, so the wireless range performance will be similar, and they offer up to +4dBm transmit power if necessary.
Most protocols will need to spend time searching…
Other Parts Discussed in Thread: CC2571
Hello everybody,
I want to set up a BLE network, with one central node and several other peripheral nodes. What should I buy?
The mini development kit and than separately keyfobs as slaves? Is it possible to build…
Other Parts Discussed in Thread: CC2571 , MSP430G2231 I have started designing CC2571 ANT break out board using the reference design provided by the Texas instruments, and i want to interface that board to MSP430G2231 to send the sensor value to PC using…
So I've got enough info about all these SoCs and WNPs. But WNPs need a MSP430 to work. Which one would you recommend for:
CC2541S (PREVIEW)
CC2564
CC2564-TIWI-UB2
CC2570
CC2571