Part Number: CC2530 Other Parts Discussed in Thread: Z-STACK , CC2592 Test TX Power with SmartRF Studio 7, set PA_POWER=0xF5, and get max TX Power 21dBm.
But after program our FW (HEX doc.), with same setting at PA_POWER register, only can get TX power as…
Part Number: CC2592
Hi,
page 19 in the datasheet for CC2592 (SWRS159) dated Feb 2014 states that there is a via keep out area next to pin one. That indicates to me that I must keep copper away from that area.
But as far as I can see in the reference…
Part Number: CC2538-CC2592EM-RD Other Parts Discussed in Thread: CC2538
Hello everyone,
I have set up a system with this product:
- MGM220P for EndDevice
- CC2538-CC2592EM-RD for coordinator
- RevPi Core 3+ for manage the system
All work fine…
Part Number: CC2530-CC2592EM-RD Other Parts Discussed in Thread: CC2592 , CC2530 I want to test the S11 of CC2530+CC2592 RF TX and RX chain.
Use SmartRF Studio 7 to set TX or RX mode for CC2530+CC2592, how to confirm if CC2592 is working at a right mode …
Part Number: CC2592 Other Parts Discussed in Thread: CC2530 For CC2530+CC2592 solution,
About RF_N and RF_P between CC2530 & CC2592, if they're differential trace? Do they need impedance matching ?
If yes, what’ s the impedance ?
Part Number: CC2592 Other Parts Discussed in Thread: CC2640R2F , CC2541 , CC2640 , CC2650 We are using CC2640R2F and CC2592,But we ran into trouble and we have been debugging for a month。
CC2592 is already working,But the Bluetooth signal is very difficult…
Part Number: CC2592 Other Parts Discussed in Thread: CC2530 , Z-STACK I would like to use CC2530+CC2592 solution for Zigbee, and about CC2592 PA and LNA logic, If I can set PA_EN, LNA_EN, HGM all at high logic, to enable PA and LNA at the same time? so…
Part Number: CC2592 Other Parts Discussed in Thread: CC2530 Is it a sin to route the Inverted-F antenna on the opposite side of the PCB from the CC2592? A Faraday cage will cover the CC2530 and the CC2592, but mechanical constraints yearn for the inverted…