Part Number: CC2592EMK-RD Other Parts Discussed in Thread: CC2592 , CC2520 Hello
I have two questions about CC2592 application.
1. My project needs to use CC2520+CC2592. When I refer to the reference design of CC2538-CC2592EM and CC2592EM, I find…
Hi,
Gavin Hu said: the PA output impedance is internally matched to 50 ohm, right?
Yes.
Gavin Hu said: If it is, from the below picture, those components on the CC2592 output are not used for impedance matching, right?
In the CC2592 datasheet…
Part Number: TIDC-CC2530-CC2592EMK-RD Other Parts Discussed in Thread: CC2530 , CC2592 , CC2591 Hi all,
Currently I am using CC2530 and the CC2591 in a device (in production). I received a notification saying that CC2591 is not recommended for new design…
Part Number: TIDC-CC2530-CC2592EMK-RD Other Parts Discussed in Thread: CC2592 , CC2591 hello
I tested the CC2592 Device.
Range Extender Set the CC2592 : RSSI : -65dBm
Range Extender Set the CC2591 : RSSI : -54dBm
The difference between setting…
Part Number: CC2650MODA Other Parts Discussed in Thread: CC2538-CC2592EMK , , CC2652R Hello,
can I use cc2650moda(BLE) and cc2538-cc2592emk/rd(Zigbee) together on single board??
Part Number: TIDC-CC2530-CC2592EMK-RD Other Parts Discussed in Thread: CC2530 , CC2592 Hello
I want a design review for an attachment.
and check the CC2530 GPIO for PA_EN/LNA_EN/HGM control.
I Request a software example code
zetmote1801_181228…
Hi Narendar,
The antenna is a 2.4 GHz Inveted F antenna which can be found here: www.ti.com/.../swru120d.pdf
Here is the reference design for this design: https://www.ti.com/tool/TIDC-CC2530-CC2592EMK-RD
Best regards,
Bun
Part Number: CC2592 Our design TIDC-CC2530-CC2592EMK-RD showed the range extender design for single antenna. Customer would like to check whether there are any solutions to achieve the range extender for double antennas. Could you please help check it…
Hi Usman,
The CC2592EMK-RD is a Reference Design which is not sold by TI, however the Design Files are available if you would like to build these boards yourself or investigate the layout. You should otherwise purchase a CC2538-CC2592EMK or review…
Hello Han,
What stack version and projects are you using for each node in your network? Regarding the sniffer log, ZR 0x42E6 is most likely removed since it does not complete a TC link key update. If distance or physical interferences are an issue then…