Part Number: CC2630 I see in the MAC CoP documentation information about the power control pins, and it refers to the NPI Users Guide for more details. In the users guide it specifies UART behavior when the host is or is not using these pins. I'm unclear…
Part Number: CC2630 Other Parts Discussed in Thread: SYSBIOS , TIMAC , Z-STACK ,
I am writing for an existing deployment so I cannot use the resources available in ROM. SYSBIOS and Stack has to entirely be in flash. I'm seeing that the FLASH_ONLY config …
I had some more time to carefully recheck this and it appears that my earlier analysis was wrong. The who packages behave the same. With the software bug PA and LNA sit at high, HHM at low. LNA and HGM flip to transmit.
The expected behavior is that…
Part Number: CC2630 Other Parts Discussed in Thread: SYSBIOS , TIMAC , , Z-STACK I'm writing for an application where using SYSBIOS in ROM isn't possible so I have to place a lot in flash. Unfortunately this has put me in a difficult situation resource wise…
Part Number: CC2630 Other Parts Discussed in Thread: TIMAC , CC2650 This is for an existing product so I have no flexibility in hardware, software or the type of encryption I am using.
I am writing an application for a CC2630 that requires CBC AES function…
Part Number: CC2630 Other Parts Discussed in Thread: CC2650 , TIMAC , UNIFLASH , , CC2651R3 , SYSBIOS I am working with TIMAC (tirtos_simplelink_2_11_01_09) and trying to write a simple app that blinks some LEDs. This program works as expected when during…
Part Number: CC2630 Other Parts Discussed in Thread: TIMAC , SYSBIOS
I am trying to init the ICall stack similar to the MSA example for TIMAC (I am stuck with this hardware so switching isnt possible). I am properly making the ICall calls from a task function…
Part Number: CC2630 Other Parts Discussed in Thread: SYSBIOS , TIMAC , CC2650 I am writing for an existing (deployed) hardware product that has been running a non TI RTOS solution. Due to the nature of the flash on the CC2630 I cannot write to flash addresses…
Part Number: CC2630 Other Parts Discussed in Thread: CC2650MODA ,
Dears
Can you help share the certificate file for ETSI EN 300 328 (Europe) • EN 300 440 Class 2 (Europe) • FCC CFR47 Part 15 (US) • ARIB STD-T66 (Japan)
Part Number: CC2630 Other Parts Discussed in Thread: LAUNCHXL-CC2650 , CC2650 , TIMAC , CC2652R Sorry if this isn't the best forum but once I specify it's a CC2630 I need help with the forum forces me to post here. I only need 802.15.4 and do not need Zigbee…