Part Number: CC2640R2F In CC2640R2F , Negative edge interrupt is working with the setup
user_pin | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_NEGEDGE | PIN_HYSTERESIS,
But the Positive Edge Interrupt is not working .
user_pin | PIN_INPUT_EN | PIN_PULLDOWN |…
Part Number: CC2640R2F Other Parts Discussed in Thread: UNIFLASH , Hello,
How to unlock CC2640R2F, when both Flash Prog 2 and Uniflash fail to unlock?
XDS debug probe: 3.0.0.25, 3.0.0.28
Uniflash v8.3.0, v8.6.0
Flash Prog 2 v1.8.2
(This seems to be an…
Part Number: CC2640R2F Other Parts Discussed in Thread: CC2640 Will FCC accept TI's certification for products I sell based on cc2640R2F?
Or, do I need to repeat the FCC certification process again?
Regards,
John
Part Number: CC2640R2F Hello, I have a question. I am using CC2640R2F eddystone. Is Modulation ON/OFF possible? If so, is there any reference material?
Part Number: CC2640R2F Other Parts Discussed in Thread: LAUNCHXL-CC2640R2 Hello,
I would like to ask some questions about BLE antenna matching. I designed a board and followed the balun and matching from the LAUNCHXL-CC2640R2 using the same inverted F…
Part Number: CC2640R2F Other Parts Discussed in Thread: CC2674R10 , CC2651R3 , CC2652R7 Hi,
May I know whats the range about i2s sample reate ?
Any possible to support 48khz or above?
Thanks.
Part Number: CC2640R2F I need assistance with designing a matching network to connect the CC2640R2F to a 50-ohm antenna using ADS. Could you guide me on how to model the CC2640R2F in ADS? Is there any library that I can download?
Additionally, understanding…
Part Number: CC2640R2F Hello, I have a question. Currently, I modified the CC2640r2f periperal obsever code, but the symptom is that BLE does not work once a uart message is sent. Is there a solution? uint8 rsp_data[50]; static void SimpleBLEPeripheralObserver_StateChangeCB…