Part Number: CC2640R2F Other Parts Discussed in Thread: CC2340R5 Tool/software: Hello,
I m using code composer studio version 10.3.0.00007
ble sdk simplelink_cc2640r2_sdk_5_10_00_02
XDC tool version 3_51_03_28_core
I have working code of offchip_oad…
Part Number: CC2640R2F Other Parts Discussed in Thread: LAUNCHXL-CC2640R2 Tool/software: Hi,
Currently using CC2640R2F Simple Central project. Where facing an memory corruption and sometime we seeing complete Page30 is filled with 0xFF data.
Test…
Part Number: CC2640R2F Tool/software: hello, im using code composer studio version 10.3.0.00007
ble sdk simplelink_cc2640r2_sdk_5_10_00_02
XDC tool version 3_51_03_28_core
external flash w25x40cluxig
#define DEFAULT_MAX_SCAN_RES 10
// Advertising…
Part Number: CC2640R2F Tool/software: HI Community,
I would like to upgrade my CC2640R2F SDK from simplelink_cc2640r2_sdk_5_30_00_03 to latest version simplelink_cc2640r2_sdk_5_30_01_11 .
I was using simple_peripheral_cc2640r2lp_oad_onchip_app project…
Part Number: CC2640R2F Tool/software: Hi,
Following up on a previous related thread - HW_FAIL_INADEQUATE_PKT_LEN,
I'm sharing reproduce test results by increasing the heap memory.
In conclusion, it didn't work.
We have seen improvements by adjusting…
Part Number: CC2640R2F
Tool/software:
Hello,
We are checking a sample among our products that is not working properly. We checked by dumping the flash memory to see if the flash was broken, and the code area was normal. However, the first 4 bytes…
Part Number: CC2640R2F Tool/software: Hello,
I implemented WDT in our product as the example watchdog.c.
And for testing, I called Watchdog_clear every 10 seconds and confirmed that the watchdog callback was called when 60 seconds passed by not calling…
Part Number: CC2640R2F-Q1 Other Parts Discussed in Thread: CC2564C Tool/software: Hi TI team ,
Could you help to recommend a Bluetooth module to meet the below requirement:
BT version:5.3
Dual mode(BR/EDR+LE)
Support LE audio
AEC-Q100
Operating…
Part Number: CC2640R2F Tool/software: Hello,
We have designed a BLE module based on the CC2640R2F chipset and are facing an issue when performing a soft reset or system reset in our custom firmware / application
Expected Behaviour: Reset should…