Part Number: CC2640R2L Other Parts Discussed in Thread: SYSBIOS , CC2640R2F
Hello everyone.
I bought a new mac mini and now I am with problem to build projects in my new envinroment. In my previous installation everything was working fine.
CCS …
Part Number: CC2640R2L Hi,
Since we dont have too much battery capacity so need to caculate power consumption very careful.
I need to use:
1. Use ADC to read sensor data.
2. Use PWM to generate 1 Mhz , Duty cycle 20% .(I just wanna use this…
Part Number: CC2640R2L Other Parts Discussed in Thread: CC2640R2F Hi team,
Here's the request from the customer:
The SDK version is simplelink_cc2640r2_sdk_2_30_00_28. Can the CC2640R2L run the function of AOA Receiver in the SDK?
Using 2640R2F…
Part Number: CC2640R2L Other Parts Discussed in Thread: CC2652P , hi Expert,
Is the HCI command 'ADV_RPT_INC_CHANNEL 'Supported in the CC2640R2?
BR,
frank
Part Number: CC2640R2L Hi Team,
When using the 2640 serial port, configure the callback mode and turn on the partial return function to receive an undetermined string,
normally the 2640 serial port receives a string that can be received as a packet…
Part Number: CC2640R2L Other Parts Discussed in Thread: CC2640 Hello TI Support,
I want to print all exceptions on the UART0 of CC2640R2L.
I use the following config, but it doesn't work.
app_ble.cfg
var SysMin = xdc.useModule('xdc.runtime.SysMin…
Part Number: CC2640R2L Hi. how to count a given number of external pulses with the formation of an interrupt upon completion of the count? With the possibility of battery operation. The frequency of the external pulse signal is 300 kHz. Using GPTimer…
Part Number: CC2640R2L Other Parts Discussed in Thread: CC2640 Hi ,
environment:
sdk: simplelink_cc2640r2_sdk_5_10_00_02
project: ble5_host_test_cc2640r2lp_app
I want to config cc2640 as a peripheral through BTool.
The following is my steps…
Part Number: CC2640R2L Other Parts Discussed in Thread: CC2640R2F ,
Hi,
I just got little confused about ADC between CC2640R2L and CC2640R2F.
In TRM chapter 17, looks like this is for CC2640R2F sensor controller only..
For CC2640R2L, I only…
Part Number: CC2640R2L Hi, Can you please share the following information to fill the following questionnaire requested by BQC or point me to the document where I can find the following information ? Supported Power Class: 1 ,2 or 3 ? Supported Power…