Hi Yuval,
Thank you for your patience.
I think I made some mistakes on previous tests. So I pull a new example and start it all over again.
The problem is still there: the same code works fine on the launchpad, but can not jump to oad-persistent…
Part Number: CC2640R2F Tool/software: TI-RTOS Hi All,
I am working on CC2640R2F_LAUNCHXL kit and simplelink_cc2640r2_sdk_1_50_00_58, i have tested the micro_eddystone_beacon_cc2640r2lp_app sample code on launch pad, it perfectly working fine.
Based…
Part Number: CC2640R2F Other Parts Discussed in Thread: SYSBIOS , CC2541 , CC2640 Tool/software: Code Composer Studio Hi All,
I am trying to flash and debug a CC2640R2F (RSM) with an example from the CC2640R2F SDK (simple_broadcaster) onto a custom…
Part Number: CC2640R2F Tool/software: TI-RTOS Hello,
It has been over a month now and I am stuck with the problem of waking the CC2640R2F from shutdown on my custom board. I am using the simplebroadcaster example for my project. I got this project…
Part Number: CC2640R2F Hi,
I am working on CC2640R2FRSM chipset which is 4X4, so my board file is "CC2640R2DK_4XS" this one. Now i want to add ADC in my simple_central project. So i have edited "CC2640R2DK_4XS.h" and "CC2640R2DK_4XS.C" files for ADC…
Part Number: CC2640R2F Tool/software: Code Composer Studio I am working on a custom board of cc2640r2f having the 4x4 chip. I changed the CC2640R2_LAUNCHXL.c, CC2640R2_LAUNCHXL.h, board.h with the 4x4 files and rename them to CC2640R2_LAUNCHXL in every…
Part Number: LAUNCHXL-CC2640R2 Tool/software: Code Composer Studio Hello,
I am currently developing on the CC2640R2LAUNCHXL board around the empty ccs project example. I have configured an OLED display to communicate over SPI but would like to redefine…
CC2640R2 sample code on path C:\ti\simplelink_cc2640r2_sdk_1_30_00_25\examples\rtos\CC2640R2_LAUNCHXL\drivers\ ,sample code can not to run.
What did I miss?
Thanks~~
Part Number: CC2640R2F Tool/software: TI-RTOS In simplelink_cc2640r2_sdk_1_30_00_25
Object: simple_peripheral
Use the following function to delete all the binding information, the return value is invalid value, and delete the information is not successful…
Part Number: CC2640R2F
Hi Ti,
Since we are using 4 × 4 RSM , I want to move the code from 2640R2F 7X7 to 4X4.
I refer the below doc steps to modify , but I think 2640R2F still using 7X7 board configuration.
software-dl.ti.com/.../custom-hardware…