Part Number: CC2642R-Q1 Hi engineers,
Environment: CC2642 SDK 6.30
My customer is using SPI to communicate with another device. When CC2642 is running in RX mode, sometimes it will overrun, entering this:
,
Customer tried to recover from overrun by disabling…
Part Number: CC2642R-Q1 Other Parts Discussed in Thread: CC2642R Hi All,
I am using CC2642R chipset for the Bluetooth development purpose. In this we choose Simple mesh node OAD on chip/persistent app/bim on chip base project for the Customer requirement…
Part Number: CC2642R-Q1 Hi expert,
Please help confirm if it OK to design the antenna circuit. It's a little different with the recommended circuit.
Thanks a lot!
Andy
Part Number: CC2642R-Q1 Hello team,
I have a question about the connection issue. Sometimes CC2642 BLE may inexplicably disconnect, and the reason for disconnection is 0x08 or 0x3D. I check these two error code in BLE specification doc. The Error code…
Part Number: CC2642R-Q1 Hi engineers,
My customer is facing a phenomenon. When they shutdown the device and wake it up in a very very short time, it will fail to wake up. I found in a e2e thread it says the device will take some time to shut down. It…
Part Number: CC2642R-Q1 I used 20pin Header for connecting XDS110
I imported BLE5 Stack's Project Zero to IDE
and after Run Debug Menu, appear Error - 267
Question1: Which pin on the XDS110 should I connect 3.3V?
Question2: Is Error-267 caused by…
Part Number: CC2642R-Q1 Hello Team,
CC2642 SDK version: 6.40
Use mobile connect, Write and notification data once per second,after a period of time, ATT Write Transaction not response
What may be the reason for this? Do you need to catch any logs.
Part Number: CC2642R-Q1 Hi engineers,
I'm using ATT MTU exchange in the beginning of connection established. to avoid transaction failure I remotely disconnect if MTU exchange status is not success. However, once this disconnect is triggered, I cannot…