Part Number: CC2642R-Q1 Team,
My customer who wants to employ the CC2642-Q1 for automotive product is looking for external flash device (also plans to implement the off-chip OAD). Looking for suitable to external flash device (allpies to Automotive specification…
Part Number: CC2642R-Q1 Hello,
I'm using a simple peripheral to connect to an iPhone. When the connection is established, the connection info parameters are sent through CAN to several passives. Each passive receives the connection info and starts CM…
Part Number: CC2642R-Q1 Other Parts Discussed in Thread: SYSCONFIG Hi Team,
I use writeFlash/readFlash in the simple_peripheral routine,I configured the configuration from the picture in my first question, but it was not written in, like Figure 4 .
1. …
Part Number: CC2642R-Q1
We are using the Simple Peripheral example code with all default parameters- the device is continuously advertising
We are measuring the current consumption of board by using voltage drop across a 100R series resistor
We are seeing…
Part Number: CC2642R-Q1 Hi Engineers
I'm facing a 100% reproducible issue when using UART driver in SDK 5.20
1. use a external MCU to transmit a particular packet to 2642 via UART
2. 2642 will UART_close after receiving this packet
3. MCU will wait…
Part Number: CC2642R-Q1 Hello,
I am currently facing a challenge and I hope that you guys can support me and help me solve the problem.
I use the Honor Magic 5 pro( Cell phone ) to connect and disconnect CC2642, after multiple disconnections and connections…
Part Number: CC2642R-Q1 Hi,Team
If this IC receives power of -35 dBm or higher, it will not maintain linearity and will saturate. (See the figure below.)
I am concerned that when communicating with a high power transceiver (e.g., Tx Power is +20 or…
Part Number: CC2642R-Q1 Hello,
I have the RTLS setup running with the coordinator running as a BLE peripheral, the responder working as the BLE central and 2 passives. The setup is configured to work with CAN instead of UART.
When the responder connects…
Part Number: CC2642R-Q1 Hi engineers,
I'm trying to using project zero as peripheral and pairing to a central using public address. I found after successful first bonding, central disconnect and reconnect to CC2642, I could always see a 0x3E disconnect…
Part Number: CC2642R-Q1 Hi engineers,
my customer is reporting a weird 0x3E disconnect. regarding to the spec says, the feature exchange request should be replied within 5 retries otherwise the connection will be "failed to establish". But from their…