Part Number: CC2650MODA How can I consistently enforce/determine mapping of SNV base address? I intend to use the ROM bootloader, but want to preserve BLE name. Alternatively, can I reserve a raw flash sector with the linker and read/write directly?
Part Number: CC2650MODA Hello,
I have developed a custom application which is developed from the Project Zero file for CC2650Launchpad from simple link academy 1.11. I have tested my application with CC2650launchapad and it worked fine.
I am using CCS…
Part Number: CC2650MODA Other Parts Discussed in Thread: ADS1115 , CC2640 Device - CC2650MODA
I am using a simple_peripheral example for BLE. My task is to get data from external ADC and sent it over to BLE. ADC interface and BLE code are working fine…
Part Number: CC2650MODA Other Parts Discussed in Thread: CC2650 , SYSBIOS , CC2640 , CC2652RB
I tried out the SPP server example from the BLE examples 2.2 on the CC2650 launch pad and it now after some time consuming odyssey works fine. I then tried to…
Part Number: CC2650MODA Other Parts Discussed in Thread: CC2640 , CC2650 I want to avail myself of the bootloader, and want to avoid putting anything in the last page of flash other than .ccfg. I've tried removing the mapping in cc26xx_app.cmd, but .cinit…
Part Number: CC2650MODA Other Parts Discussed in Thread: MSP432E401Y , MSP-EXP432E401Y Hi there,
We have a custom made board that includes an MSP432E401Y as main core and a CC2650MODA module to provide bluetooth connectivity. On this card, there is also…
Part Number: CC2650MODA Other Parts Discussed in Thread: CC2650 I am working with the CC2650MODA and need to communicate with a sensor that requires a data frame on the SPI bus to be 32 bits; however, I only see options on the CC2650 to have the frame…
Part Number: CC2650MODA Hello. I'm really struggling to get started with the SimpleLink product line.
I'm trying to get any kind of serial/logging output from the device back to a console. I was able to get UART working, but can't find any easy to…
Part Number: CC2650MODA Other Parts Discussed in Thread: ENERGYTRACE , LAUNCHXL-CC26X2R1 I have customized the simplePerphieral application. I used LaunchXL-CC26X2R1 with EnergyTrace to monitor power consumption. I only see the current going down to about…
Part Number: CC2650MODA Hello,
We apologize to make you rush. However, we would like to know the latest schedule for the EN 300 328 V2.2.2 certification. The deadline seems to be coming and our customer asking us the status for this.
Best Regards, Nomo