Part Number: CC2674P10 Hi team: env: 1. SDK: SimpleLink™ CC13xx CC26xx SDK 8.30.01.01
2. project: znp_LP_EM_CC2674P10_tirtos7_ticlang
3. chip: CC2674P10
I read a post on E2E ( https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group…
Part Number: CC2674P10 Hi Team:
env: 1. https://github.com/TexasInstruments/ot-ti (tag: thread-ti-v1.3-1.0)
2. Dongle(CC2674P10)
1. Flash the OpenThread RCP firmware to the Dongle and then insert it into HAOS.
2. In HAOS, after the OTBR APP…
Part Number: CC2674P10 Other Parts Discussed in Thread: SYSCONFIG My customer is using a custom board with CC2674P10 RGZ, they would like to enable the 20dBm Tx power on ZNP project, but could not find how to.
znp_LP_EM_CC2674P10_tirtos7_ticlang only…
Part Number: CC2674P10 Dear experts,
I would like to create a new project using the CC2674P10 chip with TI CCS . Could you please advise which example I should choose for a Coordinator and which one for an End Device ?
Thank you — preferably…
Part Number: CC2674P10 Tool/software: Hello,
I am using cc2674 Bluetooth chip for Bluetooth communication and we observed following issue could please support for following issue what we observed, we are facing a BLE issue in passive entry. When we…
Part Number: CC2674P10 Other Parts Discussed in Thread: CC2674R10 , CC1314R10 , CC1354P10 , CC1354R10 , CC2755R10 , CC2755P10
Q1: What security features are available on CC2674 and CC13x4 devices?
A: The CC2674 and CC13x4 (CC2674R10, CC2674P10, CC1314R10…
Part Number: CC2674P10 Tool/software: Hi Team,
May I have your comments about below question?
While the CC2674P10 works in 2.4GHz, 20dBm, use 1.8V for below power is workable or not?
Or do I need to apply 2.5V or 3.3V in 20dBm?
Thanks.
Part Number: CC2674P10 Other Parts Discussed in Thread: CC2755R10 , CC1311P3 Hello exports,
My customer is considering to use TI WCS device and they are searching a WCS device that meets the following conditions.
1. Communication distance: 500m
…
Part Number: CC2674P10 Tool/software: Hello
I run the demo "uart2echo_LP_EM_CC2674P10_nortos_ticlang",
int main ( void )
{
Board_init ();
// initUART();
/* Start NoRTOS */
NoRTOS_start ();
/* Call mainThread function */
mainThread…
Part Number: CC2674P10 Tool/software: Hi There,
I know there is no CZed power table between 10~14dBm.
I would like to ask customer to try to tune the bit.
could you please suggest which bits customer should try?
BR. Albin