Part Number: CC2745P10-Q1 Tool/software: I'm seeking to track the motion of a probe, ballpark 20cm up to about 150cm from the instrument, what sort of resolution could I achieve with TI's channel sounding solution?
Is there a ready demo I can just power…
Part Number: CC2745P10-Q1 Tool/software: Hi, TI:
We used simplelink_lowpower_f3_sdk_8_40_00_61 SDK on CC2745 platform. When we only added TrustZone module in syscfg, many errors occurred. We found that is lack of "ti/drivers/lib/ticlang m33f/drivers_cc27xx_ns…
Part Number: CC2745P10-Q1 Tool/software: Hi,
I tried to debug the basic_ble_lp_em demo, it stuck at LL_Init function. CCS version 12.8.1, SDK 8_30. Any hint? Thanks
Part Number: CC2745P10-Q1 Tool/software: Hi, Ti
We have integrated an SE security chip into the peripheral device. After initializing the Bluetooth broadcast upon startup, we need to read the local name from the SE chip and replace the original default…
Part Number: CC2745P10-Q1 Tool/software: Hi, Ti
I have currently added CCC authentication functionality to Bluetooth (using CC2340 as the central device and CC2745 as the peripheral device). The data for CCC authentication is exchanged through L2CAP…
Part Number: CC2745P10-Q1 Other Parts Discussed in Thread: UNIFLASH Tool/software: When a program that performs ECDSA and SHA256 hardware operations is written to a PG2.0 board,
SHA2_open and ECDSA_open do not become HSMLPF3_STATUS_SUCCESS in HSMLPF3_init…
Part Number: CC2745P10-Q1 Other Parts Discussed in Thread: CC2745R10-Q1 Tool/software: Hi Team,
Accroding to the ADC Buffer API doc, I have noticed ADC Buffer Driver doesn't support this now.
SDK: simplelink_lowpower_f3_sdk_8_40_00_61
My customers…
Part Number: CC2745P10-Q1 Tool/software: When using the official OAD project, the recipe for target 'post-build' failed compiler error (failed to execute the sbtool script) is as follows:
UnicodeDecodeError: 'gbk' codec can't decode byte 0xf9 in position…
Part Number: CC2745P10-Q1 Tool/software: Hi, TI:
When I use spi0 and two UARTs on CC2745, the DMA of UART1 will conflict with the DMA of SPI0 and I can't use both UARTs at the same time.
Is it possible to use spi and both UARTs at the same time? …
Part Number: CC2745P10-Q1 Tool/software: I checked the time that iCall Task is running during BLE connection and found that the task is occupied for 1~3ms at the following times. What is the processing time for each of these?
Once at the time of BLE…