Part Number: CC2745R10-Q1 Hi team,
My customer is evulating CC2745R10-Q1 on automotive application. They want to check if CC2745R10-Q1 has enough CPU & memory (flash, RAM) capability.
HW environment:
CC2745R10 will connect to 3 SPI device (Security…
Part Number: CC2745R10-Q1 Hi team,
I am running a BLE example ( car_node ) with SimpleLink SDK (v9.14.02.16).
On EVK board → works correctly
On custom board → App_StackInitDoneHandler was not triggered.
Observation
BLEAppUtil_init() is…
Part Number: CC2745R10-Q1 We used CC2745R10-Q1 as CarNode and CC2340R53 as KeyNode to test CS in Python demo, but the distance value could not be obtained.How to implement CC2745R10-Q1 and CC2340R53 channel sounding ranging on SDK9.14.10.41? How to set…
Hello,
PERABATHULA D V B KOTESWARARAO said: Is it expected behavior that OSAL APIs cannot be used before vTaskStartScheduler() ?
Yes. OSAL stands for Operating System Abstraction Layer, and serve as an abstraction layer for the underlying RTOS. In…
Part Number: CC2745R10-Q1 Other Parts Discussed in Thread: UNIFLASH Hi TI support team,
I am planning to implement the OAD function using the SDK example basic_ble_oad_dual_image and perform OAD through the TI app SimpleLink Connect .
However, UniFlash…
Part Number: LP-EM-CC2745R10-Q1 Other Parts Discussed in Thread: CC2745R10-Q1 Hi:
In studying the CAN communication function of the LP-EM-CC2745R10-Q1 development kit, do I need an additional CAN transceiver kit to test CAN communication? And what is…
Part Number: CC2745R10-Q1 We are using the CC2745R10 to measure distance with SimpleLink Low Power F3 SDK v9.10.00.83 .
When we run the system in distance mode and log the calculated distance, the result returned by the SDK is correct. However, when…
Part Number: CC2745R10-Q1 Hii Ti team We are currently using the CC2745R10-Q1 device along with FreeRTOS , and we have observed that the BLE stack supports a maximum MTU size of 255 bytes . Our application requires an MTU size of approximately 342 bytes…
Part Number: CC2745R10-Q1 Tool/software: Hi,
HW: TI CC2745R10-Q1 EVM
SW: SDK 9.12.00.19
We want to enable PTM and follow the instructions in https://software-dl.ti.com/simplelink/esd/simplelink_lowpower_f3_sdk/9.12.00.19/exports/docs/ble5stack…
Hi Eshaan,
Please see the picture for env setup (key node and car node). I am using hardware module:
LP-XDS110 (debug probe to flash)
LP-EM-CC2745R10-Q1 (evaluation module for CC2745R10-Q1)
BP-EM-CS (external board for channel sounding)