Mor,
As already mentioned in my email:
So essentially, I’ve reviewed the Vitals v3.0 schematic as if there is a CC3100 device as the target.
Is SOP2 floating? There is an X on R9. Please add a 10k pull down for CC3100.
There are X’s on the traces…
Part Number: CC3100 Hi Everyone,
Here I am looking for CC3100 SDK for MacOs , Please let me know if there are any leads.
Thank you in advance.
Chiranth
Part Number: CC3100 Hello,
Does the CC3100 support testing using the loopback address (127.0.0.1-127.255.255.255) on a specific port (e.g., 80)?
If so, how can I test if the HTTP server is enabled or not this way?
Thank you
Part Number: CC3100 Other Parts Discussed in Thread: CC3200
Hello,
If I call sl_NetAppStop( SL_NET_APP_HTTP_SERVER_ID ) to disable the HTTP Server when it is already down, does that cause an overwrite to the CC3100 flash?
Thank you
Part Number: CC3100
Hello,
We've noticed that a lot of our devices fail to respond to ARP requests.
Some devices have a 0% success rate responding to ARP requests while others sit around 85-90%.
This was determined using the arping command. E.g.: arping…
Part Number: CC3100
Hello,
How do I enable/disable the internal webpage for the CC3100? this is my version info: v1.0.1.15-2.14.0.0.
I've tried accessing it using its assigned IP but the page doesn't load.
Part Number: CC3100 Hello,
Can I get a clear explanation of the sl_GetTimestamp API? Is it necessary or beneficial to implement when using an OS?
Thank you
Part Number: CC3100 Other Parts Discussed in Thread: CC3XXXRADIOTEST Hi team, helping a customer with this issue. He would like to measure the RSSI value using these devices, and from a quick look, this looks feasible.
Are there design resources or a reference…