Part Number: CC3120MOD Hi,
we use CC3120MOD in our device.
The question is:
For test purposes like EMC testing and other Radio tool should be used, but it is possible to put the CC3120MOD in test mode via application, without using radio tool?
The application…
Part Number: CC3120MOD Other Parts Discussed in Thread: CC3120 Hi,
Is it for CC3120MOD any update in SimpleLink SDK CC3x20 service pack sp_3.16.0.0_2.0.0.0_2.2.0.7 ?
As this service pack released very frequently and I am not able to release my host control…
Part Number: CC3120MOD Dear Sirs,
we asked for ETSI EN 300 328 v2.2.2 evidence for CC3120MOD months ago and we were answered with this link: e2e.ti.com/.../925048
Our regulatory compliance people are asking if we can provide ETSI EN 300 328 v2.2.2 as…
Part Number: CC3120MOD Other Parts Discussed in Thread: CC3120 , CC31XXEMUBOOST Hello,
I want to send a burst of three messages in transceiver mode using sl_Send(). However, rapidly calling it only lets the first one through even though sl_Send() correctly…
Part Number: CC3120MOD Other Parts Discussed in Thread: UNIFLASH
Hi,
is it possible to add during image creation with UniFlash (.sli file) to add in the image user files and this image(.sli) to contain user files?
After that, when program the image to…
Part Number: CC3120MOD Other Parts Discussed in Thread: CC3120 Hi,
we are using CC3120MOD in a very low power device.
For this reason the connection to the WLAN (AP) and IP address acquisition (DHCP is used).
I tested some brands of AP (D-LINK, TP-LINK…
Part Number: BOOSTXL-CC3120MOD Other Parts Discussed in Thread: CC31XXEMUBOOST , BOOSTXL-CC3135 , CC3120BOOST , CC3120 Hi. TI.
I would like to purchase the product guided by TI at the URL below.
============================= BOOSTXL-CC3120MOD : 4EA CC31XXEMUBOOST…
Part Number: CC3120MOD Other Parts Discussed in Thread: UNIFLASH , , CC3120 Hello All,
To connect Wi-Fi module to Uniflash I need only the following pins: TX/ RX/ RST (or nHIB)
The same setup is not working with Radio Tool (I'm using CC3xxx_RadioTool_1…
Part Number: CC3220MOD Other Parts Discussed in Thread: CC3120MOD Hi all,
CC3120MOD is roughly $7 whereas CC3220MOD is $5 at 1ku pricing. Just trying to understand why it is less expensive even though it seems to have more functionality?
THanks! Lau…