Part Number: CC3130 Other Parts Discussed in Thread: CC3135 Hi
After intergrating the radiotool.c into our RX I observed that some commands are using the uart communication and some SPI.
I would hope that the commands using uart could be changed to using…
Part Number: CC3130 Hi,
We are using CC3130 in a product that combined both BLE and Wi-Fi communication.
We are using the Scan functionality of the CC in order to find the Wi-Fi networks it can connect to.
We would like to ask couple of questions about…
Part Number: CC3130 Hi
For productiontest of CC3130, we need to use some of the Radio TX/RX test commands.
So for enabling the radiotesting via SPI channel (RX65 -> CC3130), I would need to integrate the files radiotool.c + h file into my already integrated…
Part Number: CC3130 Hi we are looking for the interface protocol between the CC3130 and the Radiotool, We will need this for a Production test mode with a very reduced set of commands for RX and TX verification, we will access the CC3130 from our boards…
Part Number: CC3130
I'm studying this article now,
https://www.ti.com/lit/ug/swru458/swru458.pdf?ts=1623664712368
In the page 7,
"3.2.2 Layer 2",
These traces are return current path for the input decoupling capacitors (C11, C13, and C18…
Part Number: CC3130 Other Parts Discussed in Thread: CC3100 , CC3135 , CC3120 Hi
I've succeded in making the break signaling over uart to our CC3130.
After this I can get version and start programming the external flash.
But according to other specs…
Part Number: CC3130 Other Parts Discussed in Thread: UNIFLASH , Hi
I've made a small uart driver on the Renesas RX65, for enabling bootloadermode in CC3130 and then programming, similar as UniFlash.
I've logged UART communication when programming via…
Part Number: CC3130 Other Parts Discussed in Thread: CC3120 Hi,
I'd like to use the CC3130 as an upgrade to an existing design using the CC3120.
When I look at the latest Simplelink SDK Wifi Plugin 4.20.00.10 July 2020, for example, the service packs…
Part Number: CC3100 Other Parts Discussed in Thread: CC3130 Hi
We are using a RX65 connected via UART and SPI to the CC3130.
Since we are using the SPI for communication through TIs SDK (sl_Start ,, etc..) and we can program new ServicePackages by using…
Part Number: CC3130 Other Parts Discussed in Thread: CC3100 , CC3135 , CC3120 One of my customers would like an all-in-one smart WiFi chip with a true RTC feature that works even through power-down or reset. It is my understanding that with the CC3100,…