Part Number: CC3135 Other Parts Discussed in Thread: UNIFLASH , BQ25756 I encountered the following problems while debugging CC3135. Can you help me answer them? 1. How to query the channel where WIFI is located? 2. In the CMW100 signaling test, the 5G WIFI…
Part Number: CC3135 We port the code to ThreadX. After the port is completed, the sl_start function is stuck. In our current analysis, as described in the attached document, it appears that there is competition for semaphores. Can you give me some debugging…
Part Number: CC3135MOD Other Parts Discussed in Thread: BOOSTXL-CC3135 , CC31XXEMUBOOST TI team,
We use TI demo board (CC31XXEMUBOOST+BOOSTXL-CC3135) for adaptivity testing, use TI's software Radio Tool.
The first is thing that needs to be clarified…
Part Number: BOOSTXL-CC3135 Other Parts Discussed in Thread: CC31XXEMUBOOST Hi Sir, I am going to develop an application to send data via wifi, i have stm32L496 STM board which will read data from sensors and it transmits the data to CC31XXEMUBOOST and…
Part Number: BOOSTXL-CC3135 Other Parts Discussed in Thread: CC3135 after porting to STM32F4 with SPI interface
sl_Start success
also sl_DeviceGet sl_NetCfgGet sucess with correct chip id etc
but when calling sl_WlanConnect is always return SL_API_ABORTED…
Hi Tony,
1. This does appear to be the correct version.
2. Are you developing your project using CCS studio? Additionally, did you start by running one of the examples or were you planning to start with a new project? I would recommend starting by flashing…
Part Number: CC3135 hey, I'm Kalpesh Jadhav, i new to TI and im working on the WiFi module CC3135 as a booster pack for MSP432 MCU im using CCS stidio 12.0 for the development and getting errors saying undefined first referenced symbol in file ----…
Part Number: CC3135CC3135 supports UART and SPI, so how are these two communication methods chosen? How do I tell the chip whether I am currently choosing SPI or UART?
Part Number: CC3135 Hi,
For EMC testing purposes, I'd like to use a single frequency band (between 1 and 13) in the 2.4GHZ range. I've seen that it's possible to choose between channels 1, 6 and 11 in Access Point, but I'd like to use STATION mode for…
Part Number: CC3135 Other Parts Discussed in Thread: CC3235S , Hi,
I use the transceiver mode to test TX emission during ECM tests. It works well with the frequency channel selection. I can test from channel 0 to channel 13 but i don't see any difference…