Part Number: CC3200 Having issue in connecting to Dropbox for OTA. Facing CDN error while trying to connect by presigned url. I would like to have more information on whether the issue is with TI or I need to follow up with dropbox. Below is my device…
Part Number: CC3200 Other Parts Discussed in Thread: BOOSTXL-SHARP128 Hello,
I am trying to use an SD card to load bmp images onto the CC3200 Microcontroller board. The breakout board that I am using for this is an AdaFruit! SSD1351, which is an OLED…
Part Number: CC3200 Other Parts Discussed in Thread: SYSCONFIG Hi team,
I have read https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wi-fi---internal/f/wi-fi---internal-forum/1233489/cc3220moda-wifi-at-command?tisearch=e2e-sitesearch&keymatch…
you can't delete it, but you should be able to re-write it without a token (it was supposed to be created with "public-write" flags that enables overwriting it (note that we use a "downgrade protection" mechanism so you can only use a newer SP - that…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200SDK , UNIFLASH Hi team,
CCS:8.3.0
SDK:1.5.0,CC3200SDK_1.5.0\cc3200-sdk\example\p2p
Mobile phone model: Huawei Mate60
The program stopped in this while, the routine has not been changed…
eventually, IT guy turn off wifi 6, make only wifi 4 available, and do some strange setting, which they don't understand why they make it works, now cc3200 can access server via 9120AX.
thanks.
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200 , UNIFLASH What would be the best way to reset the target processor on a CC3200 Launchpad without reprogramming the flash ?
I've installed the latest Uniflash (8.5.0) and it seems like…