Part Number: CC3220S Other Parts Discussed in Thread: CC3200 Hello everyone
I am using the custom board my all example are working properly when i use IC (CC3200) everything is working and wifi is also working. But when i change IC to CC3220S on custom…
Part Number: CC3200 Hello Everyone,
I Have Some Question
1) How to i Know the Which Pin in Which Port? so i get ulPort
2) what is "ucPins" means GPIO or Microcontroller pin or Is it defined in any Library?
3) in SDK Blinky Example it defined…
Part Number: CC3200 Hello,
Actually, I Want NWP log file, I am Using CC3200, So I have Some Questions
1) My UART baud rate is 115200 then While Record log is it necessary to set baud rate to 921600?
2) my UART pins are different, so it is necessary to…
Part Number: CC3200 Hey Everyone,
I am trying to better understand if the CC3200 can be the base of a hardware based "phone" that will enable two remote users, each connected to a local Wi-Fi network, to
speak with one another (in full duplex…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: UNIFLASH , CC3200 Hi,
working with CCS 6.1.0 SDK1.1.0, in debug mode it works perfectly.
After I close CCS, plug off and then plugin USB, it does not work.
Disconnected jumper SO2 but it does…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200 , UNIFLASH Hi,
I am using CC3200 Launchpad, SDK1.1.0 and CCS6.1.0
No problem to develop software and debug.
Now I would like to make it work in release way.
First, I expected that if i…
Part Number: CC3200 Other Parts Discussed in Thread: UNIFLASH hello,
i am new user of TI Microcontroller, I was use cc3200 and ccs for IDE, but i Have getting some Problem. this board will not connecting to Wi-Fi or actually it not even scan the Wi-Fi…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200
I have implemented continuous ping pong uDMA in UART with wireless transmission in CC3200 but I am missing data: shown in image below, new data is not written into the buffer and thus…
Part Number: CC3200 Hi,
If I look for the vendor mac address for setting up the firewall rule,
I see a huge list of MAC address for Texas instruments. I cannot filter the TI devices on the ISE server using the MAC address.
How can I group the devices…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: ENERGIA
I am making a device to transmit data* recieved by UART continuously at 2 MHz - I have already implemented this with uDMA in PING PONG mode and the uDMA and wireless transmission* work…