Part Number: CC3220MOD I am using the CC3220MODSF12MOBR Module in a product that is going through the IS ATEX certification process. I need to know what size capacitors and inductors are inside the Module on the module laminate. Please see attachment. …
Part Number: CC3220MOD Other Parts Discussed in Thread: TLV9002
Hi,
We are Using CC3220MODSF12MOBR CONTROLLER with TLV9002 OPAMP to read the CT Voltage.
We are using Voltage based CT (20A/1V), After connecting to the Line-Load, It showing 0.115VAC by…
Part Number: CC3220MOD Hello WiFi Forum Community,
We are evaluating the use of CC3220MOD for installation on a Machine Monitoring device that measures temperature, and vibration using MEMS accelerometer among other parameters, and want to seek feedback…
Part Number: CC3220MOD Hello E2E Experts,
Good day.
Just want to verify: Does the CC3220MOD support WPA3 in AP mode?
There is supported to WPA3 in STA mode in the user guide "SimpleLink Wi-Fi CC3x20 , CC3x3x Network Processor(Rev. M) for CC3220MOD…
Part Number: CC3220MOD Hi
Check the CC3220MODS, The REACH seems not supported.
Will we support this? If yes, when will we support it?
Thanks in advance.
Part Number: CC3220MOD Other Parts Discussed in Thread: CC3220SF
Hi,
In CC3220MOD website said:
CC3220MODS and CC3220MODAx variants include 256KB of RAM
CC3220MODSF and CC3220MODASF are Flash-based MCUs with an integrated 1MB of Flash and 256KB of …
Part Number: CC3220MOD A customer found sometimes CC3220MOD hangs and they want to reset the chip as a workaround(at least before they found the root cause...). The customer would like to know if there is any risk if CC3220MOD reset every 1 second? The…
Hi,
The file I referred to is the one storing wlan profiles but it can also be other files.
These files are system files so the application does not have a direct access to these files, just indirectly via using host driver APIs.
Anyway, as the bootloader…
Part Number: CC3220MOD Other Parts Discussed in Thread: CC3200 Hi WiFi team
I have a custom board with CC32x0, used as an access-point with webserver
To perform certain operations, I send several Http POST via smartphone
With the "old" CC3200, the POST…
Part Number: CC3220MOD Hi experts,
My customer is making a board using CC3220MOD (without antenna).
Q:Pin 31(RF_BG) and GND are shorted(about 0.2Ω), is this a specification?
The first 30 of the 750 units purchased by the customer, which were initially…