Part Number: CC3220R Hi team,
Please, help me to understand what methods CC3220 supports to do WiFi provisioning.
Do we support WiFi provisioning using AP mode and a website running on CC3220 (without WiFi Starter Pro application)?
Do our SimpleLink…
Part Number: CC3220R Other Parts Discussed in Thread: CC3220SF , CC3220S Tool/software: TI C/C++ Compiler Hi Ti team:
If customer want to use the AT Command, does cc3220R must need external flash or internal ROM can support it? How large is the internal…
Part Number: CC3220SF Hi Team SimpleLink,
What is the datasheet specification for the CC3220xx GPIO Absolute Max Diode Current.. I do not see it in the datasheet. For example, see the similar spec for an MSP430 below.
Thanks, Merril
Part Number: CC3220R Hi,
As I know so far, the peak transmitted output power of FCC is 30 dBm.
The TX power of CC3220R is shown in the picture.
So I want to maximize the use of FCC standards by adding an external FEM/ PA module. The more TX power, the…
Part Number: CC3220S Other Parts Discussed in Thread: CC3220R , Hi TI Folks, Friends of E2E.
For all of those IoT makers, hardware engineers who are designing or using CC3220R, CC3220S and CC3220SF chips in your designs.
TDK has made the band pass fil…
Part Number: CC3220R Hi,
Asking on behalf of a customer:
We have an issue that makes provisioning fail if % character is present in SSID or password. I have investigated the problem and it is located in the provisioning functions supplied in the TI SDK…
Part Number: CC3220R HI Ti team:
Customers want to make a remote health data monitoring product through WIFI connection, They want to confirm what is the minimum power consumption of CC3220R under WIFI connection?
Low-Power Deep Sleep (LPDS): 135 A&Idle…
Part Number: CC3220R Hi.
We are currently developing our MPU's Firmware Update Function for Enduser's operation including CC3220R Service Pack Update.
But... , Is it allowed to Updating Service Pack on Enduser's operation?
Thank you.
Hajime…
Part Number: CC3220R Hi TI Champs.
There was an earlier thread on the query of OV798 +CC3220 , where Benjamin from TI mentioned that the development is in the works.
I have posted the thread link , below for reference.
https://e2e.ti.com/support/wireless…