Part Number: CC3220S-LAUNCHXL Hello,
I want to use CC3220 in transceiver (promiscuous) mode to communicate with each other. Means, I want to transfer custom data without wiFi connection. I have the following question.
1. What is the PHY modulation…
Part Number: CC3220S-LAUNCHXL
Hello,
Currently I am working on Smart Door lock project and the firmware is edited for our similar kind of application , I have added AWS MQTT for server communication. Now i need to enable the Power Policy.
The power…
Hi Moshe,
Could you inform me on which board revision of the CC3220S-LAUNCHXL you are using? Can you also list the jumpers you are repositioning when switching from 5V to 3.3V?
Part Number: CC3220S-LAUNCHXL Hi Support,
Below are the Sequence of steps that are followed
When the device is in Provisioning mode, i.e., in AP+SC mode, I have sent a http post request that contains the country code to be set. So, when I get the…
Part Number: CC3220S-LAUNCHXL Other Parts Discussed in Thread: CC3220S , UNIFLASH We have designed CC3220S custom board for our project. The issue is some MCUs are detecting while we check from the UNIFLASH tool. We have purchased ICs from the Digi key…
Part Number: CC3220S-LAUNCHXL Hi,
I'm trying to connect to AWS IoT Core MQTT broker (ATS type) Using FreeRTOS and TI's MQTT module (not the AWS library), but I'm getting a (-708) error on connection.
I've already changed the CA to the sf-class2-root…
Part Number: CC3220S-LAUNCHXL I followed the directions to the http server demo. Once I flash the firmware on to the development board and reset the processor I am getting a 404 error on the web server and the serial port is not reporting any data to…
Part Number: CC3220S-LAUNCHXL Other Parts Discussed in Thread: CC3220S , UNIFLASH Hello Team,
I'm posting on behalf of my customer:
I have the CC3220S launchpad board for a course at Southern New Hampshire University. The board is not working and…
Part Number: CC3220S-LAUNCHXL Other Parts Discussed in Thread: UNIFLASH Hi Experts, Good day. The customer can't use python 2 in the build system, but SLImageCreator depends on it. Is there a way to make SLImageCreator work without symlinking python to…
Part Number: CC3220S-LAUNCHXL Other Parts Discussed in Thread: UNIFLASH Hello,
I am trying to update the `mcuimg.bin` using command line as specified in `swru469h.pdf` chapter 7. Uniflash 8.3.0;
However, after overwrite, the `Certification File Name…