Part Number: CC3230S Other Parts Discussed in Thread: SYSCONFIG
Because GPIO is not enough, I want to use the 4 pins of SPI.
Does the CC323X network processor need to occupy the 4 pins of SPI ?
Part Number: CC3230S Could you describe how the WiFi Direct feature is supported in CC32xx?
Is there any known limitation?
Is there example code to use it?
Part Number: CC3230S Could you confirm (nor not) that I can connect an external eMMC Flash Memory to CC32xx and get file-level (with FAT file system) API provided by the SDK?
Part Number: CC3230S Other Parts Discussed in Thread: CC3200 We are looking at “libdecodeqr” which is used widely with MCUs for QR code scanner. Would like to know, if you have any reference / application note for QR code scanning using image sensor, either…
Part Number: CC3230S Hi!
The user's guide "Vendor Device Authentication With SimpleLink™ WiFi® Devices (SWRU547A)" tell that this feature is supported by the processors CC32XXS/SF family, but in the detailed description, the processor…
Part Number: CC3230S Hi team,
My customer recently suffers from crystal shortage, they don't have the required spec MAX ESR 70K mentioned in cc3230 datasheet. They want to know if they can use 32kHz crystal which is MAX ESR 90k Ohm. Thanks.
Regards…
Part Number: CC3230S Hi team,
About low power mode:
Low-power deep sleep (LPDS): 120 µA
Idle connected (MCU in LPDS): 710 µA
Can you show me what the difference is about above two mode? And what conditions is of the power consumption of LPDS…
Part Number: CC3230SF Other Parts Discussed in Thread: UNIFLASH
Can I use the XDS110 to connect UniFlash to the onboard CC3230?
With the attached configuration, launchpad was able to connect, but XDS110 did not.
Isn't xds110 firmware ver3.0.0.13 uploaded…
if you are using an external host and want to communicate with the NWP through SPI - you can use CC3130 which is an NWP only device (without the M4 MCU).
CC3130 support both UART and SPI as the host interface. You can start by checking SIMPLELINK-SDK-WIFI…