Part Number: CC3230SF Other Parts Discussed in Thread: CC3235SF SDK version 7:
I have used TI examples from the network_terminal project to read the RSSI value and the below code, both return the same value = -55
SlWlanGetRxStatResponse_t RxStatRespon…
Part Number: CC3230SF Using SDK- 7
I am implementing a watchdog function and reading a thread event response by pinging each thread.
After a couple of pings, the Mailbox post data corrupts, I have checked the input parameters, and it looks good till it…
Part Number: CC3230SF Other Parts Discussed in Thread: ENERGIA I want to place an image on external flash with bootloader.bin, application.bin, and factory.bin. Is it possible to customize the TI provided default bootloader to choose between loading the…
Part Number: CC3230SF Hi,
Work environment: simplelink-7
I am working on OTA and there is a need to call sl_NetAppDnsGetHostByName twice. I see the first call I make it works and returns - IP address, The connection close successfully and in another instance…
I don't know what do you mean by that. There is no specific low power feature for wi-fi scanning.
You can read more on the scanning in the programmer's guide (see chapter 4.7).
Part Number: CC3230SF I am using simplelink sdk version 7 and compiler 1240.
I am working on application code where the application copies the another application to RAM and executes it.
__asm(" .sect \".text:Run\"\n" " .clink\n"…
Part Number: CC3230SF Hi, I using the MQTT-Client Example from the SDK 7.10.00.13 on a custom board. I modified the example to make a new connection to our server and the communication is done by WebSockets. To handle that communication, I implemented a…
Part Number: CC3230SF Other Parts Discussed in Thread: CC3301 , CC1352P7 Hi, Support Team
Do we have 1x1 Dual-band Wi-Fi 4 (802.11n) + Bluetooth® 5.2 combo solution?
we want replace CYW43012FC.
if any suggestion, Please advise me.
Thanks,
Best regards…
Part Number: CC3230SF Other Parts Discussed in Thread: CC3200 , UNIFLASH Currently, I am using a cc3200 which is being programmed with UniFlash 3.4. The production (application) code and factory code (test code) are being entered into /sys/mcuimg.bin under…
Part Number: CC3230SF Other Parts Discussed in Thread: UNIFLASH
Can I use the XDS110 to connect UniFlash to the onboard CC3230?
With the attached configuration, launchpad was able to connect, but XDS110 did not.
Isn't xds110 firmware ver3.0.0.13 uploaded…