Part Number: CC3230SF Other Parts Discussed in Thread: UNIFLASH ,
Tool/software:
When we flash our new product using CCS, the board works in debug mode without any problem.
When we flash our product using UNIFLASH after flashing it with CCS, it…
Part Number: CC3230SF Other Parts Discussed in Thread: UNIFLASH Tool/software: Currently im using 4 MegaBytes (4MB) or 32 Megabit external flash memory. I want to change it to 8 MegaBytes (8MB) or 64 Megabit external flash memory.
1) Can I do that…
Part Number: CC3230SF Tool/software: Hi everyone,
I've been working with Hibernate and have utilized both available 32-bit retention registers (at addresses 0x4402FC20UL and 0x4402FC24UL ) to store values.
I now need to store additional variables…
Part Number: CC3230SF Tool/software: I know the maximum recommended flash memory size for this MCU is 32Mbit. Can I increase it to 62MBit or even higher? I know it hasn't been tested, but will it work?
Part Number: CC3230SF Other Parts Discussed in Thread: UNIFLASH Tool/software: Hi team,
My customer said the CC3230 currently supports up to three power tables. They want to clarify if this is still the case, or if there have been any updates to support…
Part Number: CC3230SF Tool/software: Hi All,
I am using the CC3230SF and need to access the serial flash file system to update my application's configuration. My device is already connected to an LTE modem, so I must ensure the Wi-Fi radio does not…
Part Number: CC3230SF Tool/software: This MCU requires jumper connectors for JTAG (for debugging) and XDS_UART_TX and XDS_UART_RX for code flashing . The jumper connectors are huge and don't fit into the enclosure. How do I flash code in the production…
Part Number: CC3230SF Tool/software: I want to use GPIO30 to do the ADC function. My battery charger's output is connected to GPIO30, and I want to measure the battery level using GPIO30. Can anyone guide me on how to do that?
Based on the datasheet…
Part Number: CC3230SF Tool/software: Hello, I am currently using SimpleLink SDK version 7.10.00.13 with my CC32xx device.
As you can see in my attached image, my current certificate catalog is very old — it is certcatalogPlayGround20160911.lst from…
Part Number: CC3230SF
Tool/software:
Hi,
I have one of my MCUs set up in AP mode, and on the other, I am trying to connect to the AP using the 'network terminal' example from the SDK. The issue I am currently facing is that although I can connect…