Hi Toshio,
toshio kubota said: We think that it is possible to rewrite the Flash(sFlash) of CC3235MODAS via the MCU, and the original circuit connects the pins of FLASH_SPI of CC3235MODAS to the MCU. So, can the Flash inside CC3235MODAS be rewritten from…
Part Number: CC3235MODAS Other Parts Discussed in Thread: UNIFLASH Hello,
According to datasheet page 15, FLASH_SPI_CLK is input,
but according to datasheet page 34, FLASH_SPI_CLK is output.
Which is correct?
I think FLASH_SPI_CLK is output from specification…
Part Number: CC3235MODAS Other Parts Discussed in Thread: CC3235MODS , CC3235MODSF Hi TI
I have the following questions:
For the CC3235MODS/MODAS module where is the user application (code execution) stored?
I think only in sFlash 32Mb. Am I right?
For…
Part Number: CC3235MODAS Other Parts Discussed in Thread: CC3235MODSF , SYSCONFIG , CC3235SF , CC3235S Hi
I am currently debugging a product using CC3235MODAS. Prior to that, we are evaluating a functional prototype using Launch-CC3235SF in parallel. I'm thinking…
Part Number: CC3235MODAS Hi,
We have used the Cloud OTA example as a reference and using a Github for a OTA. But we are getting the below error in case " OTA_RUN_ERROR_SECURITY_ALERT " sometimes.
OtaRunStep: FATAL ERROR from Ota_run -21004 !
…
Part Number: CC3235MODAS Other Parts Discussed in Thread: CC3235MODS
I'm using cc3235MODS module for L2 level N:N communications in transceiver mode. I have three issues:
The customer site is using 5GHz channels higher than 177. When I set rf channel…
Part Number: CC3235MODAS Other Parts Discussed in Thread: LAUNCHCC3235MOD , CC3235S
Hi E2E Experts,
I developed PCB with that module and i need the module will fill that tasks:
Task 1 - Communicate with MS Azure Cloud via HTTPS Rest API with OAuth 2.…
Part Number: CC3235MODAS Other Parts Discussed in Thread: , CC3220SF , CC3220S Hello,
How are you?
We are building a product with CC3235MODAS. It will be controlled by an host mcu by AT commands (firmware from SDK example at command with ti rtos). We bought…
Part Number: CC3235MODAS Hi,
I am using the mqtt_client demo code as reference. As given in MQTTClient_ConnParams server address should be either in URL or IP form and it working fine, but on client site there is a local server for that we have to use the…