Part Number: CC3235MODS Hey team,
Was wondering if there was a cross for the SX-PCEAX-SMT RF Module, intended to have a combo of BLE 5.2 + WiFi 6/E, with 2 MHF4 Connectors for antennas. I got a similar-ish product to cross-reference to CC3235MODS but wanted…
Part Number: CC3235MODS Hi Team,
As shown in the figure, there is an error when the IAR simulation is downloading.
Is there any need for short-term connection on the development board, and how to set it in the project?
Regards,
Susan Ren
Part Number: CC3235MODS Hello,
We posted questions and received recommendation from TI for the 6 layer routing of custom board in this thread:
https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1093127/cc3235mods-custom-pcb…
Part Number: CC3235MODS Thanks to valuable comments from this forum, I'm on the final stage but still have some issues.
I'm using cc3235MODS module for L2 level N:N communications in transceiver mode. I have three issues:
When I send a packet to…
Part Number: CC3235MODS Other Parts Discussed in Thread: CC3235S , CC3200 hello,
I used CC3235MODS and would like to add the WD reset capability.
reading the TRM, I came across this requirement but it also had a note that the CC3220 variants do not need…
Part Number: CC3235MODS Hi,
Could you please tell me if the CC3235MODS modules has undergone ANSI C63.27-2017 testing? If yes, then where I can I find the reports?
it seems not included in the zip files of the following link
www.ti.com/.../SIMPLELINK-CC3XXX…
Part Number: CC3235MODS I'm using CC3235OMOD in transceiver mode for factory automation application.
I was able to set GPIO mode as 'dynamic' using comon.syscfg at CCS version 10.4.0 But I found no dynamic mode at CCS version 11.1.0.0.11 I need…
Part Number: CC3235MODS Dear TIers,
I am trying to flash the CC3235MODS module using FLASH_SPI_* pins and Cheetah SPI Host Adapter.
1) In Total Phase Flash center, I cannot find MX25R3235F in the target device list, could you please provide me with the…
Part Number: LAUNCHCC3235MOD Hi,
I am recently brought a LaunchPad CC3235MOD am using the External USB110. The Main problem is Code cannot store Flash it's just a compile and Execution level.
I want the Information About How to my code is run and…