Part Number: CC3235SF Champs:
I need the image which can help to pass the
EN300.328 / V2.2.2
EN301.893 / V2.1.1
Does the RadioTool project: ==>radiotool_CC3235SF_LAUNCHXL_tirtos_ccs can pass those 2 certification?
If no, may you provide the…
Part Number: CC3235SF Other Parts Discussed in Thread: UNIFLASH 1. The constantly illuminated photo of D7. 2. The screenshot showing BootLoaderError from UniFlash. 3. The issue has been investigated (SOP is 0-1-0, TX/RX is normal, reset is ineffective…
Part Number: CC3235SF Using network_terminal in SDK 7.10.00.13 for CE Adaptivity certification, 2.4G mode EN 300 328 passed, but 5G mode EN 301 893 failed.
The CPERF Tool provided in References 16 of the swra681 file can only connect to 2.4G APs and…
Part Number: CC3235SF Hi,
I am using CC3235SF Launchpad out-of-box example program. I noticed when I am using my Android phone to save my WiFi router profile at AP mode I can only see the 2.4 GHz WiFi SSID.
However, If I use station mode both my desktop…
Part Number: CC3235SF Other Parts Discussed in Thread: UNIFLASH ,
Hi,
I have a CC3235SF Launchpad. I am trying to program the out of box example program using Uniflash. I followed this guide below for the Uniflash then added the www folder and files…
Part Number: CC3235SF Hi,
I am not able to import CC3235SF out of box example program to CCSv20.5 Theia workspace. I thought CC3235SF is supported by latest CCS version?
-kel
Part Number: CC3235SF Hi,
I have CC3235SF Launchpad running with out of box example program. I am not able to provision using SimpleLink WiFi Starter Pro Android app. The App can not even select my WiFi network.
-kel
Part Number: CC3235SF Hello Experts,
When creating a file to write to the CC3235SF using CCS, do the 4 bytes from address 200 indicate the data size?
Thanks in advance!
Regards,
Imazu Keichiro
Part Number: CC3235SF Hi,
I am using Out of Box example program from SDKv7.10. I set the domain name to www.cvd2500.net and cvd2500.net but, it is not recognized at internet browser. I change the domain name at ConfigureSimpleLinkToDefaultState(). …
Part Number: CC3235SF I have a CC3235SF device. It had been working in the field for a week. Then, communication with the device was lost. The user LED flashes once every time the device is turned on. When I unplugged the device and plugged it back in…